Part Number: BQ25856-Q1 Other Parts Discussed in Thread: BQSTUDIO Hi, Team
My customer Shinry is using BQ25856-Q1 in Robots application.
And Shinry want to know if they would like to change the ICHG/IPRCHG by register, could you kindly provide the…
Part Number: BQ25856-Q1 Hello, we plan to use the BQ25856-Q1 to make a battery charging product. However, during testing, the ADC readings of the BQ25856-Q1 differ from the actual measurements taken with a multimeter, as shown in the table below. Could…
Part Number: BQ25856-Q1 Hi,
Is it possible to parallel the outputs of multiple BQ25856-Q1 battery charge ICs together?
During the CC phase it seems like they would all share the load equally, but in CV mode it is not clear what would happen since…
Part Number: BQ25856-Q1 I have a design in process that uses an ideal diode controller to OR the output of two BQ25856. Is this likely to confuse the control loop in the BQ25856?
Part Number: BQ25856-Q1 Hi Team,
Want to double check with you, Tj and Ta are same in BQ25856-Q1 is same in the datasheet, any reason why Tj is same as Ta? For my understanding, Tj should be higher than Ta for some calculation Tj=Ta+Rthermal. Please…
Part Number: BQ25856-Q1 Other Parts Discussed in Thread: BQ25756 Tool/software: Hello,
Is there a calculations sheet available for the BQ25856-Q1. I see there is one linked on the web page but it is for a different chip. Are these parts close enough…
Part Number: BQ25856-Q1 Other Parts Discussed in Thread: BQSTUDIO , , BQ25750 A circuit was designed for charging a 15V/60F supercapacitor module composed of six 3V360F cells connected in series, with an input voltage of 24V, charging current of 5A, inductance…
Part Number: BQ25856-Q1 Other Parts Discussed in Thread: TPS4800-Q1 , BQ25853-Q1 , LM74502-Q1 Can the BQ25856-Q1 handle a 100A discharge current and 20A charging?
Please note that using the internal Power Path is not possible in our architecture because…
Part Number: BQ25856EVM Other Parts Discussed in Thread: BQ25856-Q1 I'm working on a new layout using the BQ25856-Q1. It would be helpful to have schematic and board layout files for the EVB as an example. Would it be possible to get access to these files…
Part Number: BQ25856-Q1 Other Parts Discussed in Thread: BQSTUDIO , EV2400 I am using the BQ856-Q1 EVM and all related accessories needed to troubleshoot and alter settings within the BQ management software. My team and I have been adjusting the hex values…