Part Number: BQ25890 May I ask how I can determine whether the chip is charging normally, by reading registers or by GPIO interrupts, such as STAT status. But now I use STAT as The condition for determining whether The charging line is inserted. For example…
Part Number: BQ25890 Dear Team,
Our customer have a question about BQ25890, BQ25890 has a shipping mode that can be used, Is there any usage limit or usage suggestion for shipping mode? We want our products to enter shipping mode when they are idle…
Part Number: BQ25890 We want a lower voltage threshold, but after 3.4V we are unable to charge our battery while this would be a OK threshold our battery supplier says.
Part Number: BQ25890 1) If short D+ and D-, which path will go based on below diagram?
2) For adjustable high voltage adapter, the output raised to 9V/12V. Does it mean the IC SYS pin output 9V or 12V? It will damage battery (3.7V).
Part Number: BQ25890 Hi team,
Here's an issue from the customer may need your help:
The circuit built by the BQ25890 cannot be charged. Devices other than the typical circuits recommended in the datasheet are not soldered. SATA always outputs a…
hi I'm Chang, xian jizhong engineer. I have some question about bq25890 and hope to get your help.
1. My system is Android 7.1. Is there a bq25890 driver for reference. 2. It identified as unknown adapters,When the voltage is lower than 3V. 3. Do you…
Part Number: BQ25890 Other Parts Discussed in Thread: BQ25892 Dear Team,
Do we have any solution with charge current < 1A and with QON.
Many Thanks,
Jimmy