Part Number: BQ25895 Hello!
I'm creating a charger for 2 Li batteries . Each of which can be added and removed during the charging process(max 2.1Ah).
The input voltage can vary 5-12V (determined by BQ25895 or ...).
The charging current of each battery…
Part Number: BQ25895 Other Parts Discussed in Thread: BQSTUDIO Hi
BQ25895 uses a 12V 15W monocrystalline solar panel to charge a single 18650 lithium battery. However, when I use the computer USB port to charge, it shows that the charging is normal.
…
Part Number: BQ25895 Hi
I have a query need your help.
At the same time, charge the battery at 3A, sys and PMID at 2A. Can the chip withstand it? How high can the chip temperature be?
Waiting for your reply.
Thanks
Star
Part Number: BQ25895 Regarding the IC BQ25895, I'm using this IC to power management which managed by MCU and provide power for Linux board. I noticed that when I use the battery and connect a 12V input source, the measured VBUS is approximately 11…
Part Number: BQ25895 Hi,
I've got a BQ25895 that won't turn on when VBUS is applied. If I manually turn it on via QON, it accepts VBUS and charges normally. No faults, registers look normal. However, when in shipping mode, it is not detecting…
Part Number: BQ25895 Hi! I notice when my battery reaches 150-200mV towards the chargeTerminationVoltage, I get interrupts every ~40 ms with no faults (fault reg reads 0). I assume this is telling me the charge is complete, however my unloaded battery voltage…
Part Number: BQ25895
Dear TI experts,
My customer wants to find the way to set with the status of D+ and D- pins are floating.
Is there any way to set charging current up to 2A using register setting or something else while D+ and D- pins are floating…
Part Number: BQ25895 Hi team,
Customer system stops charge when charging through BQ25895 from USB adapter (5V, 1A) because VBUS have a transient drop below 3.8V, Customer want to know how to recover charging after VBUS go back to 5V, they don't want …
Part Number: BQ25895 Hi Team,
Could you please let me know for BQ25895 REG02, FORCE_DPDM bit.
Will this be set as well if the AUTO_DPDM_EN is enabled and then USB plugged in?
In short, is the REG02.1 status solely for force_dpdm detection or works for…