Part Number: BQ25895 Tool/software: Hello,
please I need help with this problem:
I have BQ25895 set in OTG mode and I use boost.
I am not using VBUS yet, so there is no voltage on VBUS.
I use the default registry settings.
Electronics…
Part Number: BQ25895 Other Parts Discussed in Thread: TPS566238 , Tool/software: Q1. Can I get 3.3V from the VSYS pin to power my board? If not, can I use TPS566238 (at VSYS) to get 3.3V, 2A? Any other better suggestions to replace TPS566238.
Q2. Is…
Part Number: BQ25895 Tool/software: Hello all,
I have configured the BQ25895 to use the ILIM pin to set my input current limit to 1.5A. IINLIM is set to 3.25A. D+ and D- are shorted in my implementation since I do not need USB compatibility.
If I…
Part Number: BQ25895 Other Parts Discussed in Thread: BQ25896 , Hello!
I'm creating a charger for 2 Li batteries . Each of which can be added and removed during the charging process(max 2.1Ah).
The input voltage can vary 5-12V (determined by BQ25895…
Part Number: TPS61022 Other Parts Discussed in Thread: BQ25895 , , BQ25890 , TPS2121 Tool/software: Hi,
I am using the TPS61022 for 5V 3A boost from the SYS output of my BQ25895. I wanted to get a schematic check of the whole circuit and would love…
Part Number: BQ25895
Tool/software:
The correct value for this bit after reset is
0-Disabled as I see in Figure 8.18
or
1- Enabled As I read in Table 8-8. REG00
SLUSC88C – MARCH 2015 – REVISED OCTOBER 2022
Part Number: BQ25895 Other Parts Discussed in Thread: TPS3897 Tool/software: Dear experts,
I just found out that the BQ25895 disables BATFET whenever I plug in my battery with hesitation. If I plug it in smoothly, it powers right up. It is not a problem…
Part Number: BQ25895 Other Parts Discussed in Thread: BQ25638 , TPS61088 Tool/software: Hi!
Ive designed a custom CM5 carrier board and it seems to work well except on unplugging VBUS power in the Pi which is powered via 5V PMID shuts down. I think…
Part Number: BQ25895 Tool/software: Hi,
A couple questions - I was reading through some of the older posts and was a bit confused about the input current limit and what to appropriately set it to. Some posts made me think it was the lower limit? which…