Part Number: BQ25895M Other Parts Discussed in Thread: BQ25638 Tool/software: Hi Team,
We found BQ25895M is too hot when charging current at 5A. Could you please suggest a charger IC with lower Rds-on MOS integrated? Thanks.
Part Number: BQ25895M Tool/software: Hi, TI expert
We have received an inquiry from a customer regarding the use of the BQ25895M Charger IC.
We would like to inquire about cases where Not Charging occurs in the Charging Status register under REG0B Register…
Hi Garrett Kreger
for the time being, I have not successfully captured the status information of unsuccessful startup, except for the waveform of BTST pin which may be as described in the question, no obvious anomalies have been found on several other…
Part Number: BQ25895M Other Parts Discussed in Thread: BQ25629 Tool/software: Dear TI experts,
My customer considers BQ25895M for their new project.
The application is like external battery pack. They want to make 5V output with Li-ion battery pack. …
Part Number: BQ25895M
Tool/software:
Dear TI experts,
My customer tests BQ25895M in their own PCB, and there is a problem of detecting input source.
They are testing with HP laptop, and some ports have a problem detecting CDP. The scenario is as bel…
Part Number: BQ25895M
It is clear that the conditions for the end of charging are that the voltage meets the set 4.17v and the charging current is less than 64mA. However, the charging time of the BQ25895M charging IC is close to 12 hours, of which there…
Part Number: BQ25895M Other Parts Discussed in Thread: BQ25895 The device fails to charge a flat `liPo battery (flat , 0V as the isolation circuit in battery has isolated the battery as volage is below 3V).
The datasheet says it puts 100mA into a shorted…
Part Number: BQ25895M Other Parts Discussed in Thread: BQ25895 One of the features of the BQ25895M over the BQ25895 is PFM mode for the boost converter, to improve low-load efficiency.
However, I don't see any reflection of this in the BQ25895M data sheet;…
Part Number: BQ25895M Hi,
I am using BQ25895M with a generic 5V Vbus input source and not a USB 5V input source.
How do I connect D+ D- and DSEL pins?
I am not using any USB handshake protocol as it is not a USB charger I am plugging into Vbus. It is…
Part Number: BQ25895M Hello,
I have a project where I need a USB-UART Bridge (CP2102N-A02-GQFN28) to program and communicate with the MCU over USB. In a second project I use a MCU (ESP32-S3) with integrated USB functionality. In both cases I want the BQ25895M…