Part Number: BQ25895M Other Parts Discussed in Thread: BQ25895 Please help to check the operation behavior of BQ25895M
Boost mode operates when battery present and without any input source. Is it correct?
When input source plug in via VBUS(Assume 12V…
Part Number: BQ25895M Other Parts Discussed in Thread: BQ25890 Dear Sir,
We are testing OTG overcurrent limit and short to GND in boost mode.
but there are no protection for current limit and short.
I find just temperature protection for boost mode in…
Part Number: BQ25895M I really need to get past the glitch that occurs on PMID output, between the time that VBUS gets disconnected and the Boost Mode is operational. This seems to be at most a 30ms dip from about 5V to about Vbat, then back up to about…
Part Number: BQ25895M Other Parts Discussed in Thread: BQ25895 I'm using BQ25895M with an on-board 5V regulator providing power to the VBUS input (because outside voltage too high for BQ25895 as well as previous gen board using BQ24160R).
It keeps going…
Part Number: BQ25895M Other Parts Discussed in Thread: BQ25890 Dear Sir,
BQ25895M have Boost mode Current Limit Reg but it is reserved.
We can use to set other setting value or you have planning to release the register?
Hi,
For layout, please visit
https://e2e.ti.com/support/power-management/f/196/p/735311/2715274#2715274
https://e2e.ti.com/support/power-management/f/196/t/790169
Please see the FAQ below.
https://e2e.ti.com/support/power-management-group/power-management…
Part Number: BQ25890 Other Parts Discussed in Thread: BQ25898 , BQ25896 , BQ25895 , BQ25898D , BQ25898C , BQ25892 , , , BQ25895M
Hi,
When only the battery is present, ADC monitoring works only when the battery voltage is above the MINSYS register setting. The…
Part Number: BQ25895M Dear TI member,
When BQ25895m is used in boost mode(OTG enable and PMID=5.1V), and battery is discharged status.(no adaptor or USB in)
I have changed TS input to low temp and high temp using resistor during boost mode, then I find…
Part Number: BQ25895M Other Parts Discussed in Thread: BQ25895
I have a design with the three above components connected. I am using a 1.5A 12V charger to charge the battery. Sometimes I am getting a reset of the fuel gauge such that it forgets the programmed…