Part Number: BQ26100 Other Parts Discussed in Thread: TMP1827
Tool/software:
To evaluate the use of BQ26100 as a battery anti-counterfeiting IC, we need an instruction set or demo code for the chip. Could you please provide it; Four pages of 32x8-bits…
Part Number: BQ26100EVM Other Parts Discussed in Thread: BQ26100 , , EV2400 Dear Friend!
I have a problem about program the OTP of BQ26100 by using the EV2400+BQ26100EVM.
I can read out all the data of 5 pages OTP, also can read and write about the…
Part Number: BQ26100 I have the software running and the EV2300 connected to the EVM. I know its a good lash up as I can read the contents of memory using the DATA tab.
I cannot seem to grasp the operation of the KEYPGM button. I see the Message0 and…
Part Number: BQ26100 dear
.
200pcs of encryption program failure test passed, and 17pcs of encryption was found to be defective in retest
12 PCS BQ26100 replaced new one, and burning procedure is OK
2. 5pcs reburning procedure become OK attachment…
Part Number: BQ26100 Hi team,
When using BQ26100 communication on the one-wire Chip DS2484, For the SDQ value, ViL input low-level voltage and IOL output low sink current, is it possible to config the value by one-wire?
Best Regards,
Gene
Part Number: BQ26100 Hi Team, we just want to confirm if the BQ26100 and BQ29700 would work on LiFePO4.
Battery: Headway 38120S
Charger: Support LiFePO4 Batteries
Thank you very much.
Regards,
Mark
Part Number: BQ26100 Hello Ti-Team,
we using the BQ26100 in a application combined with the EV2300 and the "EVSW for bq26100 and bq26100EVM" Software.
The combination is ok for a few pieces, what are our options for a higher volume?
Is it possible…
Part Number: BQ26100 Hi Team,
For DSP C28346, the program files are stored in external flash chip. Do we have any instructions about how to realize the encryption of program files using BQ26100? Or, you have other recommendations.
Thanks!
Bell
Part Number: BQ26100 Hi Team,
BQ26100 provides SHA-1 engine based HMAC, however, my customer needs SHA-3. Do we have a device supporting SHA-3 based authentication?
Thanks! Roy Hsu