Part Number: BQ26200 Other Parts Discussed in Thread: BQ24105-Q1 , BQ25171-Q1 , LM51231-Q1 Dear Team,
E-CALL has been evaluated to operate in an environment of -40 to 85 degrees Celsius. We will use nickel metal hydride battery pack. I hope the charging…
Other Parts Discussed in Thread: BQ26200 Dear sir,
I am working on smart battery using your Circuit BQ26200. I have some Doubts with it
1) Is it is possible to do calibration using power supply or we have to use cell pack .
2) and what are the steps…
Other Parts Discussed in Thread: BQ26200 Dear Sir
Presently i am working on BQ-2019 one of your fuel gauge IC (For 2s). Now I want to change my IC with bq26200 IC. After referred from your datasheet,I am in doubt that how it can be use for 2S Li-ion…
Me too. I have the same problem. I'm using msp430g2553 with battery monitor bq26220.
I put the pull up resistor 10k for HDQ wire.
When I try to debug from msp430 to bq26220, the code stops in function HDQBreak();
Could it be a software problem?…
Other Parts Discussed in Thread: BQ2019 , BQ26200 Dear sir
i am working on Bq2019 and want to replace it with the BQ-26200 can you tell how to calculate the value of Rom and Ram file?
Regards
Tanvi Verma
Other Parts Discussed in Thread: BQ26200 , BQ27000 , BQ27200 Hi
We looking for Cheap Coloumb Counter for Battery Sysytem.
And we found about BQ26200 Colonb Counter for Sinngle Cell .
This device for Single Cell only, but we thinking this dveice…
Hi Engineers,
I am trying to comunicate 1-wire HDQ devices from a FPGA, and i have problems with the coms in the HDQ wire, because it only works with the lead of the osciloscope. The FPGA's pin used is configured as open drain, as the datasheet…
Hello all,
Everything is runnig ok in my HDQ code, except flash commands and clear register..
What i have to do to read one byte from Flash or RAM ?
Regards,
Leandro
Other Parts Discussed in Thread: BQ26231 Hi.
I have question for ba26200 and bq26231 for Shunt Resiter setting.
Now we thinking this Shunt Resister 0.02 ohm change to 4m ohm or under 2m ohm.
Can possible change about this shunt resister vale…