Part Number: BQ27010 Hello Sir:
We have question on BQ27010, when operating in low temperature the tape current threshold is changed.
If the PKCFG[0]=1, does the IMIN decrease by 25% per degree below Toff of 12 degrees?
Please help to provide…
Part Number: BQ27010 Hi Team,
i have customer is the old design and continue to order, but the customer is ordering BQ27010DRKRG4,
we want to know BQ27010DRKRG4 and BQ27010DRKR is the same?
Part Number: BQ27010 Hello, we are having a problem with corrupt registries in the BQ27010 we believed may be caused by spurious RF on the HDQ line introduces from the working environment. Our (1S1P) packs work in a high RF environment and recently we…
Part Number: BQ27010
From TI BU comment that the bit[INIT] can’t be cleared by Host, but it is can clear this bit[INIT] easily by using TI tool. Please double confirm with BU does the way to clear bit [INIT] is reasonable or not?
As below is the test…
Other Parts Discussed in Thread: BQ27010 Hi
I am using bq27010 gas gauge for one of my project. The battery am using for the project is Li-Polymer with 600mAh. I want to show the charge status in the LCD.when i put a new battery at first the gauge shows…
Other Parts Discussed in Thread: BQ27010 I am having a problem with the bqJunior gas gauges in that occasionally I get a battery back from the field that is reporting a very high chip temperature (reported die temperature). The temperature being read…
Other Parts Discussed in Thread: BQ27010 , BQ27320 , BQ27220 Hi Team,
BQ27010 is under design stage for an application on hand held terminal. The customer is facing an issue while programming the BQ27010 gauge device.
The procedure for programming…
Other Parts Discussed in Thread: BQ27010 I am having an issue with a battery pack using the bq27010 bqJunior gas gauge chip. The pack is initially programmed with the LMD set to 1736mAh (EEPROM value 0x26). After the first learning cycle the LMD drops…