Hello George,
Please refer to page 13 of the bq27010 of the datasheet regarding the different command bits that can be sent to the gauge. The command bit FRST requests a full reset of the gauge. This bit is located on the Mode register, address 0x01.
…
Other Parts Discussed in Thread: BQ27010 I have read the RAM memory by HDQ, But someitme the value is of the temperature is 246 celcius, That is a false measure. I have note that the temperature sensor is inside of the BQ27010. Why is the reason that the…
Other Parts Discussed in Thread: BQ27010 We have a big problem. Some EEPROM parameters of the bq27010 fuel-gauge were not set properly during production. ( The charge termination taper current threshold is too low. The charge termination voltage threshold…
Other Parts Discussed in Thread: BQ27010 Hi
I am using BQ27010 to monitor battery capacity for primary Lithion battery. there is no charge activity in this application.
with my load at a constant discharge rate, the reported time to empty is about 40%…
Other Parts Discussed in Thread: BQ27010 Hello
The bq27010 datasheet indicates it senses the end of charge by sensing a low charging current (TAPER current), setting IMIN=1 and then setting NAC = LMD.
If you are using the bq27010 as a gas gauge for…
Other Parts Discussed in Thread: BQ27010 , BQ26220
Good Morning,
I am working on BMS that's requires high coulometric measurement accuracy, two battery IC monitor devices (Bq27010) and Bq26220 (21)) sould be implemented. I would like to…
Other Parts Discussed in Thread: BQ27010 , BQ26220 Hello
Has anyone used a bq27010 as a gas gauge for a NiMH battery pack?
We were going to use a bq26220 as a monitor for a 6cell NiMH battery pack. dMax suggested we use a bq27010 as the monitor.
We…
Other Parts Discussed in Thread: BQ27010 Team-
ESP and the TI Web Site lists the BQ27010 as supporting a 2S cell configuration. However, I don't see any application literature documenting the appropriate way to configure this- Can the BQ27010 truly gauge…
Other Parts Discussed in Thread: BQ27010 Hi,
I am trying write a software for battery monitoring chip BQ27010.
I do not have HDQ interface on the host hence I am using the UART interface.
I am not able to understand how to send the command to slave…
Part Number: BQ28Z610 Other Parts Discussed in Thread: BQ27010 , BQ27000 Tool/software: Linux Hi Sir,
My project use bq28z610 gauge in android device(linux kernel 4.4). I know bq28z610 gauge driver is bq27xxx_battery.c, but bq28z610 can not met some battery…