Hello;
I included a bq27210-G2 into my new test design, and at this point I just have to use it to read the battery voltage (the rest is coming next month).
All I am getting back from the chip is 00.
Can anybody send me a few lines of code that work? …
Other Parts Discussed in Thread: BQ27210 Hi,
I've got a ASUS Eee PC 701SD laptop with an original battery pack that uses BQ27210 for management. Original cells had died and, being a guy with a DIY spirit, I decided to try to replace them with new cells…
Other Parts Discussed in Thread: BQ27210 , BQ27421-G1 my requirement is to monitor 72mAh battery.
1) can i use bq27210 as battery monitoring chip?
2) if yes what would be EEPROM configuration in order to work properly.
3) what would be the sense resistor…
Other Parts Discussed in Thread: BQ27210 I always get usb error when i run the app on win7 64 bit. I have already installed the 64bit driver for ev2300 and bq27210.
Other Parts Discussed in Thread: BQ27210 , BQ27410-G1 , TPS65720 Hi,
I have a question about the bq27410-G1 and bq27210 gas gauges. I try to decide which gas gauge to use. I have a 130mAh LiPo built in battery in my application. The pack only integrates a…
Other Parts Discussed in Thread: BQ27210 Hello,
I have custom code and am trying to use the bq80xRW1.ocx control to communicate using I2C with a bq27210. I have verified that the proper pullups are used and that commuication is working with the EV2300…
Other Parts Discussed in Thread: BQ27210 , BQ27010 , BQ27200 Is there a programming guide for the bq27210 (such as "application report slua338" for the 27200)?
And, is the 27210 a drop in replacement (hardware&software) for the 27200?
Thanks…
Other Parts Discussed in Thread: BQ27210 Hi Team!
I had a few questions regarding the BQ27210.
Looking at the datasheet, it says "An EEPROM offset value can be programmed to compensate for contributions to the DSCC offset due to the PCB layout." I am…
Other Parts Discussed in Thread: BQ27210 I'am building an electric scooter and need the SOC of bq27210 change to 100% every time the charger stops becasuse the battery is fully charged.Anybody can help me?.Thank you.
Other Parts Discussed in Thread: BQ27210 We are using bq27210 in an opamp powered configuration as per figure 1 of SLUA387 example. The battery is a 12S NiMH pack (10-18.5V), feeding an appropriate divider. The voltage seen by the gauge is in the 2.3 to 4…