Part Number: BQ27220 Hi team,
Customer is using BQ27220 in their AR project.
Their charger current setting is 1.4A, and they could see the current from the charger ADC; while some of their chip read back from BQ27220, the current is -5mA, it shows…
Part Number: BQ27220 Hi everyone,
I am attempting to update the Design Capacity on a BQ27220 gauge via I2C using the MACData block (0x40 - 0x5F), but I am encountering a checksum mismatch error. Even though I write the new data and my calculated checksum…
Part Number: BQ27220 Other Parts Discussed in Thread: GPCCEDV , BQSTUDIO Hi, TI expert
The customer intends to apply the BQ27220 to a portable terminal product.
1. Test Environment
1) Conducted tests configured as shown in the attached "Test Configuration…
Part Number: BQ27220 Other Parts Discussed in Thread: BQSTUDIO Hi Team,
I am working with the BQ27220 fuel gauge and writing calibration parameters (CC Gain and CC Delta) directly into Data Memory over I²C.
I am able to successfully update CC Gain…
Part Number: BQ27220 Hi,
I intend to use the bq27220.
I would like to know the current resolution.
Are my following calculations correct (ADC verf = 80mV) ?:
Part Number: BQ27220 Hi TI Team,
I am working with the bq27220 fuel gauge and configuring the EDV thresholds through MCU firmware during initialization.
I updated the EDV thresholds to:
EDV2 = 3200 mV
EDV1 = 3000 mV
EDV0 = 2900 mV…
Part Number: BQ27220 I am working with the BQ27220 ROM-based fuel gauge and am encountering an issue where all RAM-based parameter updates (specifically Design Capacity) are lost during a Power-On Reset (POR). While I understand this is a ROM-based gauge…
Part Number: BQ27220 Hi,
We put a BQ27220 as fuel gauge on our beacon system.
We are experiencing a strange self consumption of the gauge circuit when the system is completely off, e.g battery is supplying the gauge and we analysed the current profile…
Part Number: BQ27220 Other Parts Discussed in Thread: GPCCEDV Hi,
I use the bq27220 as fuel gauge and I want to use the BTPDischargeSet() to trigger an interrupt when battery goes low.
But as you well know battery capacity depends highly of temperature…
Part Number: BQ27220 Hi everyone,
I am having trouble updating the Data Memory on the BQ27220 . Specifically, I am trying to update the Design Capacity at address 0x929F , but it appears the gauge is not accepting the data writes to the MACData block…