Part Number: BQ27320 Other Parts Discussed in Thread: GPCCEDV , GPCCHEM Hi Team,
My customer would like to design BQ27320.
1P1S ,2000mAh,4.35V.
Gauge is in the main board.
Would you please provide comment on how to config the gauge?
BR,
…
Part Number: BQ27320 Hello,
I am using this part to monitor my LIPO battery. The Gauge needs a sense resistor in series with GND.
I have the battery mounted in some clips, that means that positive terminal and negative terminal are not together…
Part Number: BQ27320 Hello,
I am using a 3350mAh Battery with the BQ27320. This battery can go as low as 2.7V, but my device only works if the minimum battery voltage is 3.3V.
If I discharge my battery from 4.2V (FULL) to 3.3V, the used capacity is…
Part Number: BQ27320 Other Parts Discussed in Thread: BQSTUDIO Hello, I am using a BQ27320 with an external NTC resistor attached to a battery.
Right now the UI (Ev Board+BQStudio) only responds to the internal temperature sensor of the Gauge, I have…
Part Number: BQ27320 Other Parts Discussed in Thread: BQ25180 ,
Hello, I designed a custom board using the BQ27320 and a BQ25180 as BMS. I am monitoring some strange behavior in my board and can not find where the problem might be.
A USB is used as…
Part Number: BQ27320 Other Parts Discussed in Thread: BQSTUDIO I am using the Ev Board to monitor the current from a Battery. When I edit the settings for the Gauge in BQStudio they don't upload to the Board. How do I upgrade the new settings to the Gauge…
Part Number: BQ27320 Other Parts Discussed in Thread: GPCCEDV , BQSTUDIO , GPCCHEM Hello,
I really want to understand the Battery Capacity that the IC detects.
Step 1) Configure an initial Battery Capacity, from the battery datasheet. This value is…
Part Number: BQ27320 Other Parts Discussed in Thread: BQSTUDIO Hello,
I am using a BQ27320 to monitor the SOC of my battery. My Device has a PIC24 microcontroller. I already configured and tested the Gauge with the EV Board and BQStudio and exported…
Part Number: BQ27220 Other Parts Discussed in Thread: BQ27320 , , BQ27520-G4 Hi Team, What is the main difference between BQ27220 and BQ27320? These are both CEDV but I want to know how to decide which device to be selected. Best Regards, Yaita
Part Number: BQ27320 Hello,
I am writing a driver for a BQ27320, using the Technical Reference Manual (SLUUBE6A, March 2018) and can not find description of the DEVICE_NAME subcommand in section 2.1.x. How many bytes should it return? Is the subcommand…