Other Parts Discussed in Thread: BQ27410-G1 , BQ27220 Hellow.
The BQ27410-G1 is used with the structure shown below.
It outputs the SOC value normally at idle (0.8A).
Active (1.3A) normally outputs the SOC value, but it suddenly greatly decreases.
After…
Part Number: BQ27410-G1 Other Parts Discussed in Thread: BQSTUDIO Hi.
I'm using BQ27410 and trying to use GPOUT pin to detect battery low status.
To do this I set OPCFG.BATLOWEN bit. and it is working as expected.
But, I want my device work more in…
Part Number: BQ27410-G1 Hello Everyone, We are using a BQ27410 fuel gauge in our product. When the device is bootup after the battery is inserted, the first boot always gives the value of POWER_SUPPLY_CHARGE_FULL_DESIGN=1000000.
Our battery capacity is…
Part Number: BQ27410-G1 Hi Team,
Our customer is looking for the linux driver for this part. However, the bq27xxx driver does not support bq27410. They tried to modified some code of bq27421 to support bq27410, but SOC is still get zero or 100 only.
Cana you…
Part Number: BQ27410-G1 Dear TI.
I have questions in Datasheet of bq27410.
Command code of OPCFG in "Table 5. Extended Commands" is 0x3a / 0x3b.
Q1. Does this(0x3a / 0x3b) mean that OPCFG is 2 bytes?
But, in "Table 8. Operation Configuration…
Part Number: BQ27410-G1 Hi team,
Issue: In the application system circuit, the MCU is shut down when the system is shut down, so there is no MCU to communicate with the BQ27410. Will the BQ27410 work properly if the battery is charged now? For example…
Part Number: BQ27410-G1 Hi team,
The customer has the following 3 questions may need your help:
1. What is the default cell chemical ID for the BQ27410?
2. The customer's cell is Panasonic's NCR18650B, 3350mAh corresponds to TI's established Chemical ID…
Part Number: BQ27410-G1 If the battery is never discharged fully (or even below 70%), will that cause the fuelgauge's learned capacity (Full Charge Capacity) to drift over many cycles?
I've have seen from our logs that after a few charge-discharge…
Part Number: BQ27410-G1
Hi,
After I swopped batteries on my product I do a Factory Reset and then 2 battery cycles. The battery cycles have been working fine for very long but if I do the factory reset first then SOH and Remaing Capacity shows as 0 for…
Part Number: BQ27410-G1 Other Parts Discussed in Thread: BQ27441-G1 , , BQ27510-G3 , BQ27520-G4 , BQ27510-G2 , BQ27510 The BQ27410-G1 is NRND. Recommended replacement is BQ27441-G1. Both devices reside on the System Main Board.
The difference is that the BQ27441…