Part Number: BQ27411-G1 Other Parts Discussed in Thread: BQSTUDIO ,
Tool/software:
Hello,
After learning cycle I create one otfs-file with the bqStudio.
I follow the same procedure given in the document /cfs-file/__key/communityserver-discussions-components…
Part Number: BQ27411-G1 Other Parts Discussed in Thread: BQSTUDIO , EV2400 Follow up on the previous thread, the manual SLUA801 is examined and the recommended workflows for the extended commands are implemented.
Situations mentioned in the previous thread…
Part Number: BQ27411-G1 Hi all. Thanks for your time.
I have tried to use a BQ27411-G1A to monitor a battery. The interaction with the component is performed by a microcontroller via i2c.
The standard command works fine. However issues were encountered…
Part Number: BQ27411-G1 Other Parts Discussed in Thread: BQSTUDIO , , GPCCHEM Hi,
I have been trying to complete the learning cycle for BQ27411-G1 evk with a 950mAh LiPo battery. The learning cycle is performed using bqStudio in Automatic mode, with a Relay…
Hi Daniel,
We would recommend either decreasing the charge current since this could help the voltage not return to the flat region as it is above, or to include the taper current.
Regards,
Anthony Baldino
Part Number: BQ27411-G1 Other Parts Discussed in Thread: GPCCHEM Hi
We are designing in the BQ27411 Fuel Gauge into an IoT product. The battery being used for the product is given below
Lithium Cobalt Oxide 3.7V Cell voltage 630mAh capacity 4.2V Charge vo…
Part Number: BQ27411-G1 Other Parts Discussed in Thread: BQSTUDIO , Hi
I am using BQ27411-G1C fuel gauge. I am measuring current of 52mA in fuel gauge at the same time the multimeter readings show 30 mA. I am using shunt resistor of 10 milli Ohms with a…
Part Number: BQ27411-G1 Hello,
I'd like to know if BQ27411 may be used with regular Li-ion batteries, besides LiCoO2 batteries mentioned on BQ27411 datasheet.
Best wishes,
Newton Bomeisel Cardoso
Part Number: BQ27411-G1 Other Parts Discussed in Thread: BQ27542-G1 , , BQSTUDIO Hello TI Team,
We were using battery fuel gauge part No: BQ27542-G1 and now since TI is not promoting this part, we got suggessition to use part number BQ27411-G1 which is best…
Part Number: BQ27411-G1 Hi,
we are planning to use BQ27411 (or similar) as a fuel gauge.
The discharge current will be PWM with 2kHz and Imax 1,5A.
The data sheet says ADC conversion time is 1s.
Will the pulsed discharge current lead to big inaccuracy…