Part Number: BQ27421EVM-G1A Hi,
I wanted to start a Learning Cycle on the BQ-27421G1A Battery Gas Gauge. Initially I discharged my battery at a C/5 Rate to 3300mV, and then let it relax for 6 Hours.
At the end of 6 Hours, It gave us an error saying…
Part Number: BQ27421EVM-G1A Tool/software: TI C/C++ Compiler Hi
In i2c communication, I got volatage and temp exactly.
But AveraCurrent(0x10) respond FF 7F
What's wrong?
Thanks in advance?
Part Number: BQ27421EVM-G1A having issues with the sense resistor on this chip blowing. Have seen 4 failures in the last 3 weeks. What is the peak current rating for the sense resistor on this part? Can't locate it in the spec.
Part Number: BQ27421EVM-G1A Other Parts Discussed in Thread: EV2400 While reading the all resistors from BQ27421EVM with EV2400, can not able to read the configuration details of the fuel gauge IC. and showing following error:
Part Number: BQ27421EVM-G1A Hello,
I am attempting to program this gas gauge with a microcontroller and following the instructions laid out by a few manuals. I have successfully read all of the registers in the block that I want to edit and written…
Part Number: BQ27421EVM-G1A Other Parts Discussed in Thread: BQ27510 We are using removal battery of design Capacity 5200mAh. Finding issue while reading remainingCapacity & fullChargeCapacity. Now using the sample code for bq27421.
Issue is when reading…
Part Number: BQ27421EVM-G1A Other Parts Discussed in Thread: BQSTUDIO Hello,
I have been utilizing a gas gauge to keep track of the capacity in a 2600mAh battery. This means that I program the design capacity to be different from the non-volatile preprogrammed…
Part Number: BQ27421EVM-G1A All,
I am attempting to redundantly ensure that I do not lose learned data about my battery when the battery is low. In case the gas gauge does lose battery, I was hoping to be able to reprogram in qmax and the Ra table values…
Part Number: BQ27421EVM-G1A Hello,
I am using this gas gauge and configuring it on startup of a board via i2c. My issue is that sometimes the chip configures and other times it does not. It is seemingly random, and occasionally has to do with me plugging…
Part Number: BQ27421EVM-G1A Hi,
I'd like to ask which parameter will be updated during operation in Calibration class. From my evaluation, I think that only Board Offset, Int Temp Offset and Pack V Offset are updated during operation as below. Is my…