Part Number: BQ27426 Other Parts Discussed in Thread: BQ25150 , Tool/software: Hi we are developing a wearable device that uses the BQ25150 power management IC and wanted to add a more precise fuel gauge. We selected therefore the BQ27426.
It seems that…
Part Number: BQ27426 Other Parts Discussed in Thread: BQSTUDIO Tool/software: Hi team,
Could you help check if BQ27426 could support 5mohm sense resistor?
To achieve this, what software/register should customer change to meet this requirement?
Thanks…
Part Number: BQ27426 Other Parts Discussed in Thread: EV2400 , BQ27427 , BQSTUDIO Tool/software: Hello,
I was wondering if I could get a step by step guide on how to configure the BQ27426 for batteries smaller than 100mAh, I have a EV2400 for the configuration…
Part Number: BQ27426 Tool/software: I read the Quick Start Guide and TRM and learned that the taper rate allows bq27426 to synchronize with the battery’s charge termination point (i.e., the fully charged state).
If the product application consistently…
Part Number: BQ27426 Tool/software: Hi Team,
This is a Realme mobile phone project, using BQ27426.
Since the battery BTB is hot during charging and the BQ27426 is located on the back of the battery BTB, will this arrangement affect the accuracy or…
Part Number: BQ27426 Tool/software: Hi,
We use the bq27426 in your EVB and the battery management studio .
Only Battery is connected to Evb and I2c cable and there is no load connected,
The FG is in sleep mode according to the battery management studio…
Part Number: BQ27426 Tool/software: Hi there
VatChgTerm is set incorrectly in our app(Should be 4400mV, but incorrectly set to 4252mV), causing the FCC to drop on first charge. We measured it and the FCC dropped, but the RM did not.
May I ask if there…
Part Number: BQ27426 Tool/software: Hi,
We use the bq27426 in our design.
When the device is OFF, we have a low power consumption, and the Fuel Gauge is in NORMAL mode.
We measure the input current of our device with a current logger connected in series…