Part Number: BQ27427 Other Parts Discussed in Thread: BQSTUDIO Dear TI Support Team,
We are developing a custom C application on an embedded Linux host to perform a Learning Cycle for the BQ27427 directly via I2C (we are not using bqStudio). We are…
Part Number: BQ27427 Using BQ27427 initialized it at the startup to set the battery capacity to 120mAh , Chem ID to 4.2 Then applied soft reset
After the setting these coniguration , the full capcity didn't return 120mAh So, We applied learning cycle…
Part Number: BQ27427 Other Parts Discussed in Thread: BQ25190 , , BQ27220 , BQ27426 , BQ27Z758 Hello,
We would like to charge a battery and power our circuit using the BQ25190. We also want to incorporate a component capable of acting as a fuel gauge…
Part Number: BQ27427 Other Parts Discussed in Thread: BQSTUDIO I am testing a custom PCB which uses a BQ27427. The battery is a 2500mAh Li-ion battery. Most configuration settings remain the same, however, I've made the following changes
State
Design…
Part Number: BQ27427 Other Parts Discussed in Thread: GPCCHEM We currently use the BQ27425-G2A on a current design we have in production. We are re-designing the device and we would like to understand if we should move to the BQ27427 for the future development…
Part Number: BQ27427 Other Parts Discussed in Thread: BQ25190 , BQ27426 , Hello,
We would like to charge a battery and power our circuit using the BQ25190. We also want to incorporate a component capable of acting as a fuel gauge into our system. With…
Part Number: BQ27427 Other Parts Discussed in Thread: BQSTUDIO Dear TI Support Team,
We are currently trying to perform a life cycle calibration of the BQ27427 using BQStudio, but we have not been able to complete the process successfully.
We installed…
Part Number: BQ27427 Other Parts Discussed in Thread: GPCCHEM , GPCRB , BQSTUDIO Hello TI Support,
We are using a BQ27427 fuel gauge in a single-cell Li-ion battery application and are seeing a significant SOC estimation issue during low-temperature…
Part Number: BQ27427 Other Parts Discussed in Thread: EV2400 , BQSTUDIO Hi team,
We are using BQ27427 battery fuel gauge in our design. This is our first time using the fuel gauge. So could you help us in configuring it for the below battery specifications…
Part Number: BQ27427 Other Parts Discussed in Thread: BQSTUDIO , BQ27Z561 I need information about the BQ27427 data flash Summary.
We use Battery Manager Studio to test different battery profiles and we sniff the I2C bus.
We noticed that using some…