Part Number: BQ27441EVM-G1B
Hi, I am using u-boot (version 1_2020.04-r0) on i.MX8M mini and BQ21441EVM-G1B. I am facing issue to implement driver of BQ27441 in u-boot.
Is there any driver for the bq27441 that is used in u-boot? or are there any docs…
Part Number: BQ27441EVM-G1B Other Parts Discussed in Thread: BQSTUDIO
Hi team,
I performed two consecutive learning cycles on the same battery with bqstudio 1.3.101. Two learning cycle settings were exactly the same. The settings were based on the…
Part Number: BQ27441EVM-G1B Other Parts Discussed in Thread: GPCCHEM , BQ27441-G1 Hi everyone,
My name is amarr, Present i am working on BQ27441 Fuel gauge ic for monitoring Battery(Voltage = 4.2V, Current = 60mA) SOC, Voltage and current.
For doing…
Part Number: BQ27441EVM-G1B Hi Folks,
I am working Linux based platform and successfully bring up the FG( Fuel Gauge ) in kernel.
Now, I want to bring up same in " Uboot " also.
Is there any document available to bring up FG( Fuel Gauge ) in uboot…
Part Number: BQ27441EVM-G1B Hi,
There are many 16bit registers in BQ27441, such as SOC,
The SOC is little endian, 0x1C is LSB and 0x1D is MSB.
while Design Capacity is big endian, 0x4A is MSB and 0x4B is LSB.
What about other 16bit registers?…
Part Number: BQ27441EVM-G1B Other Parts Discussed in Thread: BQSTUDIO , , EV2400 Hi Tom,
I have the same message that the ' The detected dive is not compatible with this application! '
I have a board BQ27441EVM-G1B connecting to EV2400 version:0…
Part Number: BQ27441EVM-G1B Hello
I am doing learning cycle using GDK and BQ27441 , and how I judge learning cycle was complete correctly ? Could I judge it base on changed Ra value ?
Part Number: BQ27441EVM-G1B Other Parts Discussed in Thread: EV2400 Dears
When I used BQ27441EVM,connected Battery,EVM,EV2400 , but the SOC is display 0% ,even I configured Design Capacity,Design Energy,Terminal Voltage,Taper;
User Guide said : "When…
Part Number: BQ27441EVM-G1B Other Parts Discussed in Thread: EV2400 Hello
When I used BQ27441EVM,connected Battery,EVM,EV2400 , but the SOC is display 0% ,even I configured Design Capacity,Design Energy,Terminal Voltage,Taper;
User Guide said : "When…
Part Number: EV2400 Other Parts Discussed in Thread: BQSTUDIO , BQ27441EVM-G1B , I’m running Windows 10 on a 64-bit system with 8 GB of RAM and a 4.2 GHz processor. I just purchased an EV2400 and BQ27441EVM-G1B. I was able to successfully run 0.28 firmware…