Part Number: BQ27500-V120 Other Parts Discussed in Thread: BQSTUDIO , BQ27510 , BQ27500 Hello,
After implementing and running the DFI programming flow described in figures 8, 9, and 10 of Going to production with BQ275xx (slua449f), the gas gauge is keeping…
Other Parts Discussed in Thread: BQ27500-V120 Hello, all
Now we have some inquiries regarding remained battery information on BQ27500-V120 from our customer.
Please refer to the item below, and feedback us with your comment.
We released our production …
Other Parts Discussed in Thread: BQ27500-V120 I have production boards that use the bq27500-v120 devices with a 1.2Ah lithium polymer cell. The gauges are programmed in-circuit by a host cpu with a .dfi containing parameters, calibration and temperature…
Other Parts Discussed in Thread: BQ27500-V120 , BQ27500 I am having a problem with a batch coming off from production. We have (and have been using) BQ27500-V120 parts that we then program with v1.30 before loading our *.dfi image.
Before starting we…
Other Parts Discussed in Thread: BQ27500-V130 , BQ27510-G2 , BQ27500-V120 , BQ27500 , BQ27510 , BQ27210 , BQ27510-G3 I am reading the data sheets of BQ27510-G2 and BQ27500-V130 and the only two differences I can find are these:
* The BQ27510-G2 has a LDO integrated…
Other Parts Discussed in Thread: BQ27500 , BQ27500-V120 , BQ27500-V130 , BQ27500-V100 , BQEVSW I am fairly new to the bq27500.
After reading through the documentation on the bq27500 and using the bq27500EVM, I have a few questions.
Questions:
1. Is the…
Other Parts Discussed in Thread: BQ27500-V130 , BQ27500 , BQ27500-V120 We're just beginning production on a product we've design the BQ27500-V130 into. And we're modifying the upper battery temperature limit in-circuit using the EV2300 and your development…
If you didn't successfully finish programming the golden file into dataflash then it should stay in ROM mode even if you POR. It should still be in ROM mode for you and you can retry programming it using the updated flow assuming it still responds…
Other Parts Discussed in Thread: BQ27500 Hello,
we use the BQ27500 (v120) on a board, and we program it using the following steps:
1. We generated a .dfi golden pack with BQ Easy on prototype boards
2. Merge and convert the .dfi file with Dataflash…
Other Parts Discussed in Thread: BQ27500 , BQ27500-V120 The bq27500 data sheet (SLUS785B) shows a "Forced Sleep mode" path in Figure 5-1 page 25. My question is how to perform a forced sleep mode?
I2C communications state that if an external condition…