Other Parts Discussed in Thread: BQ27510 Hello all,
I would like to use BQ27510 to gauge the Batterie on my Board, and just reading how to use it. I decided to use EV2300 for writing the Flash and generate the golden Image but i don't really understand…
Part Number: BQ4050 Other Parts Discussed in Thread: GPCCEDV Dear Expert
We production state ,and found in low temperature test -20 degrees, low temperature capacity changes, 27% directly jump 7% analysis
I read the chinese version of application…
Part Number: BQ27441-G1 Other Parts Discussed in Thread: BQ28Z610 , BQ24295 , BQ27510 , BQSTUDIO , I am trying to configure the BQ27441-G1A for a new larger battery (2900 mAh). I have previously had this working with a smaller battery using the default…
Other Parts Discussed in Thread: BQ27510-G2 Hi, I am intersting in a battery fuel gauge to control the rate of charge/ discharge of the battery of my system.
Would it be a good option use BQ27510-G2 battery fuel gauge ?
My battery is a ion…
Other Parts Discussed in Thread: BQ27510-G2
(1)
Deciding Capacity of battery in
%:
From the data sheet of bq27510-G2 it seems that StateOfCharge( ) i.e. SOC
register represent capacity of battery charge from 0 to 100% in step of 1%.
In…
Other Parts Discussed in Thread: BQ27510
Normal
0
21
false
false
false
MicrosoftInternetExplorer4
Hello,
I’m using a
bq27510 v.1.11. The chemistry profile chosen by bqEasy (0.971)…
Other Parts Discussed in Thread: BQ27510-G2 , BQ27510-G3 Hello,
Question 1:
Minimum rated cell voltage is required by bqEasy, but my cell datasheet only gives nominal voltage (3.7V), can I use the nominal voltage as minimum cell voltage?
Question…
Other Parts Discussed in Thread: BQ27510 Hi,
I encountered an abnormal situation where the bq27510 on my system is giving zero reading for Full Charge Capacity (FCC) and Remaining Capacity (RC).
This situation remains even after the same battery…
Other Parts Discussed in Thread: BQ27510 Hello TI:
My english is very poor.There are some question about BQ27510. The Cell 0 Dod at EOC of BqEasy was 336,when the cell discharging.I don't understanding the meaning of Cell 0 Dod at Eoc.Aad the Full…
Hello TI:
I use the EV2300 test my battery.But I don't understand why the resistance of battery not update during discharging?
The application note tell me that resistance is updated in the Data flash after each 11.1% of DOD charge is exceeded.…