Part Number: BQ27520EVM Other Parts Discussed in Thread: BQSTUDIO When using the bq27520 demo board to connect our battery for temperature calibration (the TS of the demo board is connected to the temperature sensing pin of the battery), The actual battery…
Part Number: BQ27520EVM Other Parts Discussed in Thread: BQSTUDIO I have recently been using the bq27520EVM to determine the ChemID of a 3.7v LiPo battery that I am using.
I was running a charge/discharge cycle with a programmable load set to disconnect…
There is no point starting again. If you however want to start again i have sent you the link to the default firmware.
I have to emphasize that you do not have to observe update status going to 01. What you need is update status of 02.
I am having the issue that the EVM I am using is drawing 1-2mA off the battery when connected.
I know this as after having voltage droop, I used a TI A/D to sample a sense resistor with the battery.
The only connections I can see which could be doing…
Other Parts Discussed in Thread: BQ27520EVM , EV2400 Hi,
I have a bq27520EVM (HPA568 Rev. A). I am trying to use I2C communication between the Evaluation board and Arduino Uno where Arduino is the master and bq27520EVM is the slave. I have set-up the…
Part Number: BQ41Z50 Other Parts Discussed in Thread: EV2400 , BQSTUDIO , , , BQ27520EVM , BQ40Z50 Tool/software: Note - all references to issuing commands and displaying data refer to the use of BQStudio and an EV2400.
Also just to provide context…
Part Number: BQ27520-G4 Other Parts Discussed in Thread: BQ27520EVM , EV2400 , BQSTUDIO Hello All,
I have the EV2400 connected with the BQ27520EVM and I'm trying to complete the Q&A form in order to upload it to the gauge.
However, when I try I receive…