Part Number: BQ27530-G1 Tool/software: Hi Team,
We are using BQ27530 and STM32 MPU in our custom board. When we tried flashing the golden image in BQ27530 from MPU unfortunately MPU power is turned off, so fuel gauge got stuck in ROM mode.
When…
Part Number: BQ27530-G1 Other Parts Discussed in Thread: BQ24161B , BQSTUDIO Hi TI Team,
We have used BQ24161B(battery charger) and BQ27530(Fuel Gauge) in our design
In our application we are controlling battery charger from fuel gauge, so we…
Part Number: BQ27530-G1 Other Parts Discussed in Thread: BQ24161B , BQ24161 , BQSTUDIO , EV2400 Hi Team,
We are using battery charger(BQ24161B) and Fuel Gauge(BQ27530) in our design, BQ27530 has two I2Cs(one as a master and one as a slave).
Slave…
Part Number: BQ27530-G1 Hi,
In BQ27530, BSCL and BSDA are Push Pull output whereas in BQ2416x SCL and SDA lines are open drain. So, if we connect these lines directly, at the time of clock stretching SCL might be driven low by BQ2416x and BSCL of…
Part Number: BQ27530-G1
Hi, Support Team
We can't be program BQ27530-G1 and try to use EV2300 program the chip ,it will shut down when it program process.
How to fixed cannot program issue. We check REGIN and CE pins the gauge is enabled and powered…
Hi Dominik,
Dominik Hartl11 said: Did you manually update Qmax Cell 0? Because that one looks correct for a 3000mAh cell.
No, QMAX for Cell 0 is updated automatically when we ran learning cycle
Dominik Hartl11 said: I recommend to manually copy…
Part Number: BQ27530-G1 Other Parts Discussed in Thread: EV2400 , GPCCHEM We are trying to communicate with the Fuel gauge using the i2c-tools and we are able successfully retrieve couple of properties from fuel gauge like current_now, voltage_now, device_id…
Hi Mythili,
When the Update Status is changed to 0x02, how long does it take for IT_ENABLE to be disabled?
Mythili Balakrishnan said: How to proceed further for generating the golden image?
To generate the golden image file (.srec), please go to…
Part Number: BQ27530-G1 Other Parts Discussed in Thread: BQSTUDIO , EV2400 , BQ27531-G1 I'm having trouble trying to get the IC to respond. I realize that I connected Vss to the battery ground instead of the device ground. Would this be the reason for…
In SLUUA73 (pages 26, 27 description of JEITA_ISET and JEITA_VSET bits) it's also said that JEITA charging profiles are not used with BQ27530-G1. Does it mean that it's not possible to set any temperature controlled charging profiles for BQ27530-G1 at…