Other Parts Discussed in Thread: BQSTUDIO , EV2400 Tool/software: Dear TI Engineer,
We have recently encountered a significant proportion of communication issues with our BQ27542DRZR-G1 SMT production (Tested 1300pcs, defective 45pcs, defect rate…
Part Number: BQ27542EVM Tool/software: Dear Sirs and Madams,
We have continued to use BQ25742-G1.
Please let us confirm the various parameters after setting the golden image.
< Immediately after setting the golden image >
Cycle Count : 0
Full…
Part Number: BQ27542EVM Tool/software: Dear Customer
I want to read "MaxPackVoltage" in the Lifetime (Subclass ID 59) area.
Please tell me how to access it via I2C.
Can you give me an example of how to access send/receive commands via I2C?
Is…
Part Number: BQ27542EVM Tool/software: Dear sir Regarding SOHLOADI, I did the following tests SOHLOADI = -2000, after a complete discharge, SOH 100 >> 100 SOHLOADI = -7000, after a complete discharge, SOH 100 >> 93 SOHLOADI = -30000, after a complete…
Part Number: BQ27542EVM Other Parts Discussed in Thread: GPCRB Tool/software: HI TI engineers,
the IC I use is BQ27542. When uploading low-temperature data, GPRCRB TI gave me the following reply:
Warning: Rb level detected as 1. No Rb tweak available…
Part Number: BQ27542EVM
Tool/software:
Hi Sir
We have successfully completed the learning cycle. Cell capacity =2800, Remaining capacity=600mAh , why is bq27542 SOC= 16~27%?
EX:
OCV (V)
SOC (%)
3.77 V
16 %
…
Part Number: BQ27542EVM Other Parts Discussed in Thread: BQ27541-V200 , BQ26100 , BQ27541 Tool/software: I need to design a tool to verify batteries we make based on the bq27541-v200.
One of the tests will include an authentication check.
I obviously…
Part Number: BQ27542EVM Tool/software: Hi experts,
How to convert Hex_CC Gain to Data Memory CC Gain _Value from Data in Comm I2C?
Please share the relevant SOP (including instructions) and conversion formula
Thanks
Part Number: BQ27542EVM Tool/software: continue the test data discussion
I have to try other chem ID 2457, I tried to re-upload the data and re-run the low temperature test, but it still jumped % seriously. Please refer to the attachment.
NX81-P28A…
Part Number: BQ27542EVM Tool/software: Dear TI,
I have two questions and would appreciate your support in clarifying the following points:
Based on the data provided in the attachment, could you help analyze why the battery did not enter RELAX…