Part Number: BQ27542EVM Hello Sir:
We have a question on I2C bus free time.
We checked datasheet that tBUF was 66us.
But our tested result that tBUF is around 28us.
It's not meet datasheet.
Is it normal?
Please kindly give us some explanation…
Part Number: BQ27542EVM
Here, the I2C pull-up is 10k. If we do compatible design, can we pull up 2.2K here? What is the range of this resistance value? What are the main effects of choosing different resistance values? The 2C address is not limited…
Part Number: BQ27542EVM Hi TI team,
I have a question regarding the setting of SOHLOADI. Currently, the device uses a current of 7A/1Sec, 1A/1Sec, with an average current of 4A.
According to the manual, SOHLOADI should be set to the device's operating…
Part Number: BQ27542EVM Dear Expert
Our company currently has a new type of battery design and development, using BQ27542 with lithium iron phosphate battery cells, with a fully charged voltage of 3.6V. Attached are the GG files and LOG data. We are…
Part Number: BQ27542EVM
Hello.
If the battery is inserted or removed during communication between the host and the battery, SOC and SOH may become 0 (return from the gauge IC) in extremely rare cases.
Battery existence is checked every 300msec.…
Part Number: BQ27542EVM Hello,
May I ask what is the maximum write life of BQ27542's flash?
Is there any relevant documentation available?
I'm looking forward to your reply.
Thank you.