Part Number: BQ27546-G1 Other Parts Discussed in Thread: BQSTUDIO Tool/software: Hi,
We have started development using the BQ27546-G1 fuel gauge with a rechargeable lithium-polymer battery , and we would like to measure the following parameters from…
Part Number: BQ27546-G1 Tool/software: Hello,
We have finalized the BQ27546YZFR-G1 part for gas gauging of a 4.4V, 2400mAh battery. However, it is available only in a BGA package. Please help us find a similar part with a different package, offering…
Part Number: BQ27546-G1 Other Parts Discussed in Thread: EV2400 , BQSTUDIO Tool/software: Hello,
I required the drivers for the BQ27546YZFR-G1 Gas-Gauge IC.
Please provide appropriate I2C drivers for the same.
Part Number: BQ27546-G1 Other Parts Discussed in Thread: BQ40Z50 , BQ34Z100 , BQ34110 Tool/software: HI
We are planning to use the fuel gauge BQ27546YZFR-G1, we are having 3 cell battery pack which we need to connect to the main board and to measure…
Part Number: BQ27546-G1 Other Parts Discussed in Thread: BQ27Z561-R2 , BQSTUDIO
Hello,
We are currently working with the BQ27546-G1 to obtain only coulomb counts while interfacing with a microcontroller. However, we are uncertain about the method…
Part Number: BQ27546-G1 Tool/software: Hello
Is the bq27546-G1 able to measure fast change currents accuratly? We have a 300Hz rectangular discharge current.
the ic samples only with 1s intervall, so we are not sure if there are problems regarding…
Part Number: BQ27546-G1 Hi Team,
A bq27546-G1 is used in a customer board. the device resides on the system’s main board with a nonremovable battery, How should a charging circuit be connected to the bq27546-G1? Do charging chips need path management…
Part Number: BQ27546-G1 Other Parts Discussed in Thread: BQ27Z746 , BQ27Z561-R2 Tool/software: Hello,
I was curious about the life cycle status for this chip. Is this chip not recommended for new designs? When I go to the home page there are two alternatives…
Part Number: BQ27546-G1 Hi
The customer design with BQ27546-G1 , the problem is seriously hot. A lithium battery is connected between J20 and J2, and a load is added between J21 and J24. The load current is about 300mA, and U9 will heat up.
When…
Part Number: BQ27546-G1 Tool/software: Hello,
We've struggled with getting reasonable accuracy when trying to use this battery fuel gauge. Does TI have someone or would TI recommend someone who can review the application and make the necessary software…