Part Number: BQ27621-G1 Tool/software: Hello,
In one of our new product, I am planning to use BQ27621-G1 gas-gauge IC. I need following question regarding performance of the ICs.
1. What is the maximum and average accuracy of BQ27621-G1 against actual…
Part Number: BQ27621-G1 Hello,
we are using the BQ27621YZFT-G1A fuel gauge in our product, and we would like to clarify the expected behavior in our specific hardware setup.
System description
The Li-ion cell is connected to the BQ27621 through…
Part Number: BQ27621-G1 Other Parts Discussed in Thread: EV2400 , BQSTUDIO Tool/software: Dear TI Support Team,
I’m experiencing an issue with the I2C communication on the BQ27621-G1 fuel gauge.
In my current design, the I2C pull-up resistors are…
Part Number: BQ27621-G1 Other Parts Discussed in Thread: BQSTUDIO Tool/software: Dear TI Support Team,
I am currently using the BQ27621-G1 fuel gauge IC in my product for a single-cell 18650 Li-ion battery (nominal 3.7V, full charge 4.2V) . The ChemID…
Part Number: BQ27621-G1 Other Parts Discussed in Thread: GPCCEDV Tool/software: Hello,
The BQ27621YZFR-G1A is specified for batteries with maximum charge voltages of 4.2 V, 4.3 V, or 4.35 V. We have a battery with 4.4 V maximum charge voltage (LiCoO…
Part Number: BQ27621-G1 Tool/software: Hi team,
we tried to modify the value Design Capacity from 2425 mAh(default) to 1000 mAh according to the "3.1 Data Memory Parameter Update Example" charter in the bq27621-G1 Technical Reference document.
It…
Part Number: BQ27621-G1 Tool/software: Dear Team,
I would like to understand the different operating modes supported by the BQ27621 fuel gauge. Specifically, which modes can be manually set or cleared?
Additionally, when the battery-powered device…
Part Number: BQ27621-G1 Other Parts Discussed in Thread: BQSTUDIO Tool/software: Hi team,
1. If battery capacity is 1000mAh and default is 2425mAh, should we need to set the register every power cycle?
2. Regarding to Control( ): 0x00 and 0x01 command…
Part Number: BQ27621-G1 Other Parts Discussed in Thread: BQ27220 , BQ34Z100 Tool/software: Hi,
We have singel cell guage demand as below. Would you please suggest new part for us?
1. VBAT>4.6V
2. Li-ion polymer
3. System side guage not in pack…
Part Number: BQ27621-G1 Other Parts Discussed in Thread: BQSTUDIO Tool/software: Dear Team,
As per our application, we want to change the terminate voltage and set the registers that are related to battery parameters like design capacity.
So, if we…