Part Number: BQ27Z561-R1 Other Parts Discussed in Thread: BQSTUDIO , BQ27Z561 , I've created a golden image using the BQ27Z561 fuel gauge. However, our PCBs have BQ27Z561-R1 fuel gauges. The R1 version (v. 1561_1_03) is not listed in the target selection…
Part Number: BQ27Z561-R2 BQ27Z561-R2 devices from newer lots can be programmed with the same DF.FS file used for years. After programming they are sealed. Default UNSEAL keys 0x0414/0x3672 work on older lots but fail on new lots. FW version, HW version…
Part Number: BQ27Z561-R1 Other Parts Discussed in Thread: BQ27Z561 We can’t read the correct data memory value use 1561_0_04-bq27z561.bqz and 1561_2_01-bq27z561R2.bqz from a bq27z561 which FW version is 1.03. And we need to do golden learning based on…
Part Number: BQ27Z561-R2 Hi team,
Customer plan to use BQ27Z561-R2 in system side.
Their battery pack get the PCM intergrated, so it get the MOSFET in series with the battery cell. For BQ27Z561-R2 is impedance track algorithm, they wander how the…
Part Number: BQ27Z561-R2 Hi
When discharging at -10 ℃, the SOC is discharged from 0% to Term Voltage 3.4V, with a duration of more than 1H. Can you help me check how to optimize it; The attachments are GG files and low report files
LT-20260321.zip…
Part Number: BQ27Z561-R2 Other Parts Discussed in Thread: BQSTUDIO , EV2400 Hi together,
I have a BQ27Z561-R2 device which stucks in ROM Mode after a failed flash try from a MCU via I2C.
I want to recover it but no success so far.
If I scan the…
Part Number: BQ27Z561-R2 Other Parts Discussed in Thread: BQ27Z561 , Hello TI expert,
We have a project using the BQ27Z561‑R2 chip, and we found that random I2C read errors occur when the battery is used at the customer site.
We discovered that the…
Part Number: BQ27Z561 Other Parts Discussed in Thread: GPCCHEM Hi, I am currently in the learning cycle for a 4.2 V, 400 mAh Li-Po battery using the bq27z561 gauge and have already completed the ChemID process. Based on the generated reports, the preferred…