Part Number: BQ27Z561-R2 Other Parts Discussed in Thread: BQSTUDIO Tool/software:
Hi
I set voltage time to 10s, deep sleep Voltage time to 20s, wake check time 5s using BQstudio,
and still saw current spikes (~2mA) every 1sec.
According to…
Part Number: BQ27Z561-R2 Other Parts Discussed in Thread: BQSTUDIO , , GPCCHEM Last week we had several of our battery packs, that has the bq27z561-r2 fuel gauging IC, reading above 90% on the battery capacity but the voltage only read 2.7V (The battery…
Hello Priya,
Priya Joshi said: Given this constraint, is there any recommended way to stabilize or improve the accuracy of the SOC percentage under such varying load conditions?
Please reference section "4.81 Smoothing Engine"
Priya Joshi said:…
Part Number: BQ27Z561-R2 Other Parts Discussed in Thread: BQ27Z561 , BQSTUDIO
Tool/software:
Hello, Trying to confirm what 'minimally', is required. Pulling this info from a combination of the TRM and b27z561 evm guid (note this is not R2) - these…
Part Number: BQ27Z561-R2 Other Parts Discussed in Thread: BQSTUDIO , BQ27Z561
Tool/software:
Hello, Trying to manually read these data flash items to print out and confimr their set correctly. They current do not come back as the same value as read…
Part Number: BQ27Z561-R2 Tool/software: What is the difference between device type and device number? Taking bq27z7561R2 as an example, when reading device type as 6115 and device number as 1561, it seems that only the high and low bits are opposite.…
Part Number: BQ27Z561-R2 Other Parts Discussed in Thread: BQ27Z561 , GPCRB , BQSTUDIO Tool/software: 1round_verify.csv
round1_low_optimize_20250807-report.zip round2_low_optimize.zip
Hi,
Currently we have some issue with gauge BQ27z561 low temp…
Part Number: BQ27Z561-R2 Other Parts Discussed in Thread: BQ27Z561 , BQSTUDIO Tool/software: Hi, Our product use the BQ27z561 as the fuel gauge, the gauge connected to the CPU by I2C, and our OS is Linux(kernel 5.15).
During our test, we use the I2C…