Is our assumption correct that the SOH calculation formula of bq28z610-R1 is FCC_SOH / Design Capacity ?
What is the relationship between FCC_SOH and FCC? Why are they inconsistent?
What is the update mechanism of FCC_SOH?
What causes FCC_SOH to…
Part Number: BQ28Z610-R1 Other Parts Discussed in Thread: BQ40Z50-R2 Dear TI Technical Support Team,
I am currently working on a 1-cell battery pack design utilizing the BQ28Z610-R1 .
In our configuration, the SLEEPCHG bit is enabled, which is intended…
Hello
weibang yang said: 1. Can ZVCHG be set to 0V to achieve 0V charging prohibition?
-This is would charge the cell at 0V and is meant to "supports 0-V charging. It enables the hardware 0-V charging circuit automatically when the battery stack voltage…
Part Number: BQ28Z610-R1 Other Parts Discussed in Thread: BQ24196 Hello,
We are trying to characterize a cell. Our current setup is 1s1p. Cell is 2500mAh @ 4.2V. Our fuel gauge is BQ28Z610-R1. Our charger is BQ24196.
We have run the a charge / relaxation…
Part Number: BQ28Z610-R1 Hello
We are currently using a battery pack equipped with the Bq28z610-R1 fuel gauge. We have a usecase where the average current consumption is 1.6A, with peaks reaching up to 2A.
When this high-current load occurs while…
Part Number: BQ28Z610-R1 Hi,
We currently use the BQ28Z610-R1 fuel gauge in the removable battery for our payment terminal product. This product can work with or without a battery.
The fuel gauge Shutdown Voltage is programmed to be 2.5V and goes…
Part Number: BQ28Z610-R1 Other Parts Discussed in Thread: BQSTUDIO Hello, we are configuring BQ28Z610-R in bqStudio. We did not find a proper target with the attached error message. How can I get it updated?
Thank you in advance.
Kind regards…
Part Number: BQ28Z610-R1 Hello We are having trouble aligning our FCC and SOH. Our system is 1S1P. We are using a ChemID of 2024. Given the nature of our system, we don't really reach a C/10. Our current draw ranges anywhere from -25mA to -180mA. Right…
Part Number: BQ28Z610-R1 Other Parts Discussed in Thread: BQ28Z610 , GPCCHEM Hi TI FAE Team,
We are encountering an issue with our BQ28Z610‑R1 fuel gauge during Golden Image cycle‑learning. The Update Status register keeps stuck at 0x04 , and never…