Part Number: BQ28Z610-R1 Other Parts Discussed in Thread: GPCCHEM Tool/software: The BQ28Z610-R1 is configured with high temperature step-down charging. The full charging voltage is 8.648V at 0~45℃ and 8.4V at 45~60℃.
The battery starts to charge…
Part Number: BQ28Z610-R1 Hello, I have the following two questions:
1. What is the detailed definition of ZVCHG?
2. How do you enable 0V charge prohibition?
Part Number: BQ28Z610-R1 Hi team,
My customer is asking tolerance calculation of AOLD and SCD threshold of BQ28Z610DRZR-R1
As we don’t specify the accuracy range with different threshold program step, we only test TYP value in datasheet. Do we have…
Part Number: BQ28Z610-R1 Other Parts Discussed in Thread: BQ40Z50 , BQ28Z610 , Tool/software: Hello! Currently, we are using BQ28Z610DRZR-R1 on the BMS of our 2S1P lithium iron phosphate battery. During the usage, we have found that your chip adopts the…
Part Number: BQ28Z610-R1
Hello, I have the following questions and would appreciate your help:
Will setting ZVCHG to 0V achieve the 0V charging prohibition function?
If setting ZVCHG to 0V can realize 0V charging prohibition, what is the…
Part Number: BQ28Z610-R1 Other Parts Discussed in Thread: BQ28Z610 , BQSTUDIO Tool/software: Dear TI team and experts.
I designed a BMS circuit, using 2 battery cells connected in series, my circuit uses the central IC BQ28Z610, controls 2 external…
Part Number: BQ28Z610-R1 From BQ28Z610-R1 Technical Reference Manual. I would like to confirm only any 1 of these conditions (not all 4) needs to happen to then try to acquire a OCV measurement?
Figure 7-2 would indicate any 1 (not all 4) but I do…
Part Number: BQ28Z610-R1 Other Parts Discussed in Thread: BQSTUDIO , EV2400 Tool/software: Dear TI support team.
My customer has question about BQ28z610-R1.
They can not read BQ28z610-R1 by using 0x55 address.
Here is the error condition:
…
Part Number: BQ28Z610-R1 Tool/software: The BQ28Z610-R1 is configured with high temperature step-down charging. The full charging voltage is 8.648V at 0~45℃ and 8.4V at 45~60℃.
The battery starts to charge at 30℃ with 8.648V 5A, and after a period…
Part Number: BQ28Z610-R1 Hello E2E Experts,
Good day.
Even with ASCC and ASCD thresholds and delays set to the minimum (both threshold registers set to 0x00), a short circuit on the output of the circuit did not trigger the ASCC or ASCD faults. Rather…