Part Number: BQ29209 Other Parts Discussed in Thread: BQ7718 Hi Team,
In one of my customer application the maximum charger voltage is 10.5V and BQ29209 datasheet recommend maximum VDD voltage is 10V. Can 10.5V input damage the device since absolute maximum…
Part Number: BQ29209-Q1 Other Parts Discussed in Thread: BQ29209 Dear Support team,
Im planning a design for Li-ion battery management unit. In total I would like to have configuration of 2 cells in series and 4 in parallel (each cell mach current is…
Part Number: BQ29209-Q1 Hello team,
I want to increase the Rin(voltage monitor filter resistance) up to 10kohm even if response ability be sacrificed.
Is there any technical max limitation for this resistance?
Thank you.
Regards,
Oliver Kim
Part Number: BQ29209
Hello!
Our client applied to us for clarification of data code of BQ29209DRBR. Please advise what is the data code of the following marking : 209 / TI 4AI / ASFV
Here is the photo.
Part Number: BQ29209 I'm planning to use the bq2920x to balance a 2 cell battery, I do not care for the protection circuit. Can I leave the RVD, CVD, CCD out and connect the VDD directly to PACK+? Will the balancing functionality be affected? I'm space…
Part Number: BQ24735 Other Parts Discussed in Thread: BQ29209 , BQ77915 Hello everybody.
I'm evaluation this application:
battery powered board
4x 18650 cells
single cells has PCM
I need to put these cells in series
BQ24735 for charger
I've onboard…
Part Number: BQ29209 Hi TI!
My name Yuri. English is not my native language so please sorry me for mistakes.
I want to achieve as low current consumption from the battery as possible at a time when the device is not used (for example a month or so) and…
Part Number: BQ29209 Hello, I have a inquire about the protection circuit of lithium ion batteries.
I want to charge and discharge by connecting two 1cell (18650, 3400mAh) lithium ion batteries with protection circuit (PCM) in series.
At this time, we…