Part Number: BQ29312 Hi, Good day. Our customer would like to know the difference between the BQ29312 and BQ29312A. Also, they want to know if they can use the BQ29312PWR as an alternate to BQ29312APWR. Thank you. Regards, Cedrick
Part Number: BQ29312 Hello,
we use the BQ29312 for our batteries. What is the typical and maximum input current for the VCx Inputs.(VC1, VC2,VC3,VC4,VC5)?. At one input i measured >1mA with 4.2V and i think the IC on our board is damaged. I didn't find…
Part Number: BQ29312
Dear all:
Where are there bq80201dbt, bq29312apw datasheet? and the bq80201+ bq29312 power management application circuits?
Thanks!
Other Parts Discussed in Thread: BQ29312 Hi Tiers.
We designed battery-pack using BQ2084+BQ29312.
When battery-pack is not used, battery-pack's capacity is slowly decreased.
So in this case, We want to set sleep mode or ship mode.
But We don't know…
Jim
If I understand correctly, you are trying to use a 6S configuration with 3 series cells connected to one bq29312 and the other 3 series cells connected to another bq29312. These two packs will be connected in series to form the 6S pack. Is this correct…
Other Parts Discussed in Thread: BQ20Z80 , BQ29312 Is any one familiar with what increases the Max Error, when using bq20z80 and bq29312? Or with what can reset/lower the Max Error?
Other Parts Discussed in Thread: BQ29312 Hi,
My question is quite simple, how do we set the No.of Cells for bq29312 AFE.
I have gone through the bq29312 Datasheet. One line read's -
2-, 3-, or 4-Cell Configuration
In a 3-cell configuration, VC1 is…
Other Parts Discussed in Thread: BQ29312 Hello, On sluu205 (bq20z80EVM-001), page 12, is writen : the cells should be connected in following order : 4-Cell (in my case) : 1N (BAT-), 1P, 2P, 3P and 4P (BAT+). However, in BQ29312 datasheet, is writen : -0.3V…
I'm testing this circuit right now and when I remove the Li-Ion power source I notice this chip enters some kind of sleep mode. I've checked the rest of the board and the fuse is still good (as are the MOSFETs). Any advice? I'm following the block…
Maybe the BQ29312 is dead, the BQ29312A have an internal regulator pin 18. If the fuse have burn something is (was wrong). Maybe you connected the new battery inverter. You can check the Pin 1 of the BQ29312 the voltage must be battery.