Part Number: BQ29410 Hello Team,
will the BQ29410 be destroyed if, e.g. during manufacturing process, the connections between battery cells and the IC-pins VC1, VC2, VC3, VC4 are done with the wrong sequence? I guess not. Only the OUT pin may be activated…
Part Number: BQ29410 Other Parts Discussed in Thread: BQ7718 , BQ2947 , BQ7716 What are the ESD ratings for this part? The reliability/qualification tab on the product page lists ESD - HBM and ESD - CDM with the note "see datasheet". The datasheet…
Part Number: BQ29410 Other Parts Discussed in Thread: BQ29209 Dear Battery Management team
We want to search secondary Voltage protectors which have Q1 ceritication.
Do you have secondary voltage protecotors which have Q1 and 1-Cell like bq2941x?
Thanks…
The CD pin begins charging the external delay timing capacitor when an over voltage condition is detected.
Does it continue charging the timing cap after the 1.2V threshold is reached and OUT is asserted?
What is the maximum voltage this pin can reach…
Other Parts Discussed in Thread: BQ29410 I notice the BQ29410 and family are now not recommended for new designs but there is no end of life announcement.
I have just designed in this device. Should I design the part out now or should I be OK for the next…
Other Parts Discussed in Thread: BQ29410 My design uses the bq29410, which has a fixed threshold of 4.35V with a 4S pack. VDD is connected to the top of the cell stack, so max VDD is 17.4V.
What is the max voltage on the OUT pin? The datasheet shows a…
Other Parts Discussed in Thread: BQ29410 , BQ29400 sir i am designing a product and going to use second level protection,
i came across these above two IC`s BQ29410 and BQ29400, which one i should prefer? as the features are the same
pls help, thanks…
Thank you for reply.
I have find bq29412 in the bq29410 datasheet . And this mark is varistor my guess.
I am wait for experts people's answer.
Thanks PAN-M
Hello SB,
your battery pack needs match perfectly up with our bq20z4x, bq20z6x, bq20z7x and bq20z9x familes.
I would suggest looking at the bq20z45. it is our latest release, most accurate gas gauge and smallest footprint imedance track device.
http…
Other Parts Discussed in Thread: BQ78PL114 , BQ29410 , BQ76PL102 , BQWIZARD Hi everyone
I want to use BQ78PL114 + BQ76PL102 Evaluation Kit as fuel gauge for my Li-PO battery pack. I have some questions. Bq29410 is used as over voltage indicator in the evaluation…