Part Number: BQ2947 Hello,
The set/reset operation of the output is unclear regarding its behavior during a transient OV state, i.e., with oscillations.
This is significant due to the hysteresis threshold, which considerably shifts the OFF condition…
Part Number: BQ2947 Tool/software: Hi team,
What is the different between BQ2947 and BQ2945xy?
For 2 cells pack, BQ2947 and BQ2945xy, which do you recommend and why? The OVP is expected > 4.45.
Part Number: BQ2947 Other Parts Discussed in Thread: BQ4050 , Tool/software: Dear Team,
The BQ4050 is a power meter that integrates primary and secondary protection control functions.
There is a problem when applying, the secondary protection function…
Part Number: BQ2947 Dear Ti expert,
because my pcb board space limited,R13,R14,R15 and R18 these filter resistor can changed to 0402 packaging? the CD pin voltage is 5V?
have a nice day!
Part Number: BQ2947 Other Parts Discussed in Thread: BQ40Z50 A CofC confirming the part is UL recognized and possible images of the UL markings on the material or packaging.
Also needed for part# BQ40Z50RSMR-R2
Part Number: BQ2947
Hi,
The picture below shows the peripheral circuit of BQ294701, I would like to ask if the 10cell uses the three IC serial connection method to make it correct.
Part Number: BQ2947 hi Team,
customer want to check the power dissipation of the IC.
for example at condition
(V4–V3)=(V3–V2)=(V2–V1)=(V1–VSS)=4.0 V / IDD=2uA at TA = 25°C
what's the IC power dissipation? how might we compute for this?
appreciate…
Part Number: BQ2947 Hi TI experts, What's suggestion of bq2947 protector connect or setup procedure? I worry the wrong setup to cause OUT pin be high during cell1..2...3 connect.
Part Number: BQ2947 Hi Guys,
in the the datasheet is written that the bq2947 covers a OPV range from 3.85V to 4.6V and one has to select the desired OVP by choosing the correct suffix of the partnumber (for example bq2947 07 for 4.225V).
My problem…