Part Number: BQ2947 Other Parts Discussed in Thread: BQ4050 , Tool/software: Dear Team,
The BQ4050 is a power meter that integrates primary and secondary protection control functions.
There is a problem when applying, the secondary protection function…
Part Number: BQ2947 Other Parts Discussed in Thread: BQ2945 Tool/software: Hi team,
What is the different between BQ2947 and BQ2945xy?
For 2 cells pack, BQ2947 and BQ2945xy, which do you recommend and why? The OVP is expected > 4.45.
Part Number: BQ2947 Other Parts Discussed in Thread: BQ40Z50 A CofC confirming the part is UL recognized and possible images of the UL markings on the material or packaging.
Also needed for part# BQ40Z50RSMR-R2
Part Number: BQ2947 Dear Ti expert,
because my pcb board space limited,R13,R14,R15 and R18 these filter resistor can changed to 0402 packaging? the CD pin voltage is 5V?
have a nice day!
Part Number: BQ2947 hi Team,
customer want to check the power dissipation of the IC.
for example at condition
(V4–V3)=(V3–V2)=(V2–V1)=(V1–VSS)=4.0 V / IDD=2uA at TA = 25°C
what's the IC power dissipation? how might we compute…
Part Number: BQ2947
Hi,
The picture below shows the peripheral circuit of BQ294701, I would like to ask if the 10cell uses the three IC serial connection method to make it correct.
Part Number: BQ2947 Hi Team, Our customer would like to know the maximum output voltage for BQ294702DSGR. Here's the complete question to assure if this device is suitable for their medical device battery application:
Datasheet for BQ294702DSGR lists…