Part Number: BQ2980 Other Parts Discussed in Thread: BQ2982 Hello E2E Experts,
Good day.
I have two questions:
1. For BQ2980/ BQ2982 the OVP triggers at 4.475V. For the LiFePO4 battery, the nominal voltage being 3.6V, will this IC be able to protect…
Part Number: BQ2980 Hi Team,
I want to use the BQ298000RUGR to protect my 3.7V lipo battery, but I don't understand the schematic on the datasheet.
If you can you tell me, what the value of RSNS should be and what "Scale RC values for system reset…
Part Number: BQ2980 Other Parts Discussed in Thread: BQ25175 , Hi Team,
customer is looking for a protection IC with following specs. Could you please recommend a suitable solution?
Overcharge detection voltage: >4.393 (max value of BQ25175) …
Part Number: BQ2980 I need a protection circuit for a single LiIon rechargeable coin cell, with the following requirements:
* OVP: 4.3V to 4.4V
* UVP: 2.8V to 3.0V
* OCC, OCD: target draw is under 25mA. Cell needs about 50mA max cut-off for charge…
Part Number: BQ2980
Hello E2E Experts,
Good day.
I am developing a new product that will have a plug-pack (wall-wart) as the main power supply and internal battery backup. My main DC bus will be 5V which will be used to run the unit and charge…
Part Number: BQ2980 I'm using a BQ298018RUGR in a design and seeing unexpected results. Our circuit follows the EVK design, however when our design is connected to power the protection chip draws ~130mA current, almost all of it through the BAT pin. Also…
Part Number: BQ2980 Hello Sir:
Our end customer wants to select a smaller protection IC for 2S battery pack.
That needs these protections as below.
OV
UV
OT
UT
OCC
OCD
SCD
Do you have solutions?
Or can we use BQ2980 for stackable…
Part Number: BQ2980 Other Parts Discussed in Thread: BQ2982 I am looking for a single-cell Li-ion protector with overtemperature protection, and have found the BQ2980/BQ2982 series devices. After looking at the datasheet, I am a bit confused about what…