Part Number: BQ2982
Issue Description: This is a 1S1P battery pack (schematic circuit shown in the screenshot). In the current design, the power consumption in Normal mode is 130 µA, which is significantly higher than expected. According to the datasheet…
Part Number: BQ2982 Hello E2E Experts,
Would it be possible to hold the CTR line high for weeks on end? And then take it low again to resume.
The BQ2982 has UVP set at 2.8V, which is too low for a lifepo4 battery (they don't like being discharged…
Part Number: BQ2982 Hello,
I'm looking to use the BQ298216 as a protector circuit and want to know if the chip will automatically reset the FETs after a fault? Not sure if the CTR pin can do that, or if it has a built in timer to do this, or if the…
Part Number: BQ2982 Hi Team,
Posting on behalf of our customer
is it possible to place a PO for 6000 BQ298217RUGR with UV_Shut disabled?
It says this can be factory configured in the datasheet. We would like this part ASAP if this is possible. …
Part Number: BQ2982
Hi Experts,
When using BQ298217RUGR for a handheld device, I am seeing that the BMS sometimes shuts down due to an ESD event and does not try to recover despite TVS diodes.
The timing of the shutdown is almost immediate, less…
Part Number: BQ2982 Other Parts Discussed in Thread: BQ27426 Hi,
Can I share a sense resistor between the BQ29821 and the BQ27426 using highside? Polarity may not work since one is high side and one is low side but if they could share with separate…
Part Number: BQ2982 Tool/software: Hi,
Any chance I can contact TI to get a slightly different part in this table?
EAU will be 10k. For a reputable Li+ battery company.
Thanks,
Erik
Part Number: BQ2982 Other Parts Discussed in Thread: TMP63 Tool/software: I am trying to understand what thermistor I would need to connect to the CTR pin of the BQ298218 so that the battery is cut off at 60 C.
As I can understand from the datasheet…
Part Number: BQ2982 Tool/software: Hello,
we have design a BMS PCB board for lithium-ion protection (1 cell) with BQ298218 chip.
Unfortunatelly, output pins of the chip aren't able to drive the MOSFET on the PACK + line (with VCELL voltage = 4V…