Part Number: BQ34210-Q1 BQ34210IPWRQ1 : Can you please provide the Maximum junction temperature (Tj Max) and package loading for the following part number.
BQ24105IRHLRQ1 : Can you please provide the package loading for the following part number (i.e..,Package…
Part Number: BQ34210-Q1 Other Parts Discussed in Thread: BQ35100
Hi Team, seeking for some support.
We are currently using LiSOCL2 batteries, which is a Lithium primary battery. I see that BQ35100 supports this chemistry. We are also interested in the…
Part Number: BQ34210-Q1
Dear team,
The systems of our customer usually discharge about 10mA. It is written to the datasheet with "for Rarely Discharged Batteries", does even such a system not have any problem?
My customer uses LiFePO4. Is this…
Part Number: BQ34210-Q1 Other Parts Discussed in Thread: EV2400 , BQSTUDIO Hello,
In my current design I'm using the fuel gauge BQ34210 and I am having issue in the software side when it comes to the configuration/update the design capacity. I believe…
Part Number: BQ34210-Q1 Other Parts Discussed in Thread: BQSTUDIO , so title is my problem
after learning cycle , GPCpackaged update, get the report
write this
export the file DF
040802.gg.csv
then closed bqstudio
and import this 040802.gg…
Part Number: BQ34210-Q1 dear
Attachement is about BQ34210 SCH from customer , please help to check if have any potential design risks , thanks in advance 6355.y15_v1.0_0708_TI.pdf
Part Number: BQ34210-Q1 Other Parts Discussed in Thread: BQ27Z561-R2 Hell o expert,
M ay I have your confirm if BQ34210-Q1 could support 2V~3.65V LiFePO4 battery with 1.4A output? Or we have better solution for it? Thanks a lot!
Best regards,
Ann Lien
Vin…
Part Number: BQ34210-Q1 Hi,
I am trying to put the device into shutdown mode before that, I am making the device to Unseal mode. Once I send the Unseal commands, the BQ chip is not responding always the I2C busy error code is returning. When unseal command…