Part Number: BQ34Z100-R2 Tool/software: Hi, I’m Luis.
I
I’m trying to read the Device ID (0x0001) from the BQ34Z100-R2 using the HDQ interface on STM32 . The control register address is 0x00 .
However, I can’t find a clear explanation of the 2-byte…
Part Number: BQ34Z100-R2 T105-AES_learningCycle.zip
I attempted a learning cycle following the instructions in SLUA903 (Achieving The Successful Learning Cycle) and although the flags changed at each step learned status never progressed from 4 to…
Part Number: BQ34Z100-R2 Tool/software: Hi TI Team,
Greetings!!
I am using the "BQ34Z100-R2" fuel gauge, but i have some below queries on the output i am getting from the fuel gauge through 12C line.
1. Getting Clock stretching from Master as…
Also what's the proper datasheet for performing learning cycle, the one in just Bq34z100 is not correct for bq34z100-r2? The first difference i've discovered is Design Voltage, in SLUA925 it should include cells in a series, but then at texas forum post…
Part Number: BQ34Z100-R2 I have searched the data sheet, TRM, and forums, and have not found a definitive answer to this: Can the BQ34Z100-R2 I2C interface be used while the device is in the Internal 4-LED mode? (LED/COMM register set to 0x02? If so,…
Part Number: BQ34Z100-R2 Other Parts Discussed in Thread: BQ76942 , BQ34Z100 Hi, i would like to ask information related to CHEM ID selection and learning cycle.
In this application i will use BQ76942 in combination with bq34z100-r2 and the cell wit…
Part Number: BQ34Z100-R2
Hi TI Team ,
We are using BQ34z100-R2 in our 8S3P battery pack with nominal voltage of 25.6V .
We did the learning and update status changed to 06. and Ra table has been updated .
FCC and Qmax has also been updated . …
Part Number: BQ34Z100-R2 Other Parts Discussed in Thread: 4213 , BQ34Z100 Device: BQ34Z100-R2
We observed that after changing the Chemistry ID from 475 to 4213, the FCC immediately increases from approximately 5002 mAh to 5385 mAh without completing…
Part Number: BQ34Z100-R2 Other Parts Discussed in Thread: BQ34Z100 Hi,
I am using the BQ34Z100 with a 6S2P Li-ion battery pack having a design capacity of 9000 mAh.
I successfully completed the learning cycle, and the gauge learned a Full Charge Capacity…