Part Number: BQ4050 Other Parts Discussed in Thread: EV2400 , I currently prtoduce a small 12v battery using a maxim fuel guage chip. I'd like to switch to the TI BQ4050, but the cost of the EV2400 interface is prohibitive. Is there an alternative programming…
Part Number: BQ4050 Dear TI Engineer,
1) What are the differences in function between the Permanent Fail Fuse C and the Enabled PF C?
2) For Second Level Protection Permanent Fail a. When the Status is Alert, it will "Reset AFE FUSE bit", but the…
Part Number: BQ4050 Other Parts Discussed in Thread: BQ25703A , Hi TI Team,
Designing a cost-sensitive, embedded device powered by Li-ion battery pack with below details
Battery configuration: 2S2P (7.4V, 67000mAh) 18650 battery
Product does have…
Part Number: BQ4050 Hi Ti engineer
I noticed there is one AFE Protection Control item respectively in the PF Status and Settings sections of the gg file.
What is the function of the AFE Protection Control under PF Status?
Looking forward to…
Part Number: BQ4050 Dear TI Engineer,
1) What are the differences in function between the Permanent Fail Fuse C and the Enabled PF C?
2) For Second Level Protection Permanent Fail a. When the Status is Alert, it will "Reset AFE FUSE bit", but the…
Part Number: BQ4050 Other Parts Discussed in Thread: EV2400 , Hi
For the 2S1P battery pack , an ERROR is indicated in Log Status during charge and discharge data logging. I have highlighted the relevant part in red in the attached file. Please help…
Part Number: BQ4050 Hi,
We use the BQ4050 in our 2-series battery cell balancing, and now, we have no output for the circuit, we have below the MOSFET, we test the voltage of the MOSFET(D, S G):
Q21: V(D)=8V, V(G)=0V, V(S)=0V;
Q20: V(D)=8V, V…
Part Number: BQ4050 Other Parts Discussed in Thread: BQ24600 Hello guys,
One of my customers is looking for gas gauge IC.
They think BQ4050 is the best TI device for the following conditions Is their thought correct? If you have any beeter device…
Part Number: BQ4050 Hello team,
I have a quick question from my customer, may I ask what the size of the memory inside BQ4050 is? There is no mention of it on the datasheet.
Thank you.
Part Number: BQ4050 Hello,
I would like to design a BMS for the Panasonic NCA903864A cell. The battery configuration will be 1S1P, so there will be only a single cell.
When I checked the chemistry section of the BQ4050 in Battery Management Studio…