Part Number: BQ40Z50-R2 Tool/software: I want to develop a battery pack with a capacity of 100Ah using 5Ah cells in a 3S20P configuration.
If I use bq40z50-r2, the maximum capacity is not suitable for 65Ah.
Can I adjust the scale factor to use it…
Part Number: BQ40Z50 Other Parts Discussed in Thread: MSPM0G3507 , , EV2400 Tool/software: Hi,
I was trying to read the data flash with address 0x4E46 (CUV Protection Threshold) through MSPM0G3507 via i2c.
The problem is that I fail to read the…
Part Number: BQ40Z50
Tool/software:
Device: BQ40Z50 Firmware: BQ40Z50-R5 Cell Type: NCR18650GA (2.5 V ~ 4.2 V, 3450 mAh) Configuration: 4S ChemID: 2107 learning_cycle.gg.csv 4152.learning_cycle.log
I am encountering an issue where the SOC (State…
Part Number: BQ40Z50-R2 Other Parts Discussed in Thread: BQ40Z50 , EV2400 , BQSTUDIO Tool/software: We have developed a BMD circuti based on BQ40Z50. It manages 4 LIFE batteries, connected in series.
It happens that we receive a battery from the field…
Part Number: BQ25672 Other Parts Discussed in Thread: BQ40Z50 , Tool/software: Hi,
We are using BQ25672 for charging a 4 cell litium ion battery which is have bms Bq40z50.
1. Once our battery get fully depleted it enter into the discharge cut-off…
Part Number: BQ40Z50-R2 Other Parts Discussed in Thread: GPCCHEM , BQSTUDIO
Tool/software:
Hi Anthony,
We've got a situation where the pack is reporting 43% RSOC and the voltage is 13.7V
The full charge voltage for this pack is 14…
Part Number: BQ40Z50 Tool/software: Dear TI Engineer,
We encountered a problem when using BQ40Z50, that is our battery has a factory voltage of 13.22V and a charge capacity of 60%, but after installation at the customer's site, it reads a voltage…
Part Number: BQ40Z50-R2 Other Parts Discussed in Thread: BQ40Z50 Tool/software: Dear TI Support Team,
I am working with the BQ40Z50 and have a question regarding the hardware protection latch recovery condition. According to the TRM, when NR=0, the…
Part Number: BQ40Z50 Tool/software: Hi
Customers have encountered the following problems using Gauge IC BQ40Z50RSMR-R2
1.The battery percentage reading is inaccurate.
2. The Gauge IC BQ40Z50RSMR-R2 needs to be recharged and woken up each time the…