Relly Chu said: Does this mean it will affect the Gauge's calculations? And will it impact any internal parameters that update automatically, such as Cycle Count or Qmax?
For a real application, you need the gauge wait for the SoC to update, the same…
Part Number: BQ40Z50-R2 Hello,
We are currently working on the bq40z50-r2 and using a 4S3P cell configuration
In the bq40z50-R2, after the battery reaches full charge, both FC and TC flags become set, but the CHG FET remains ON and the charger continues…
Part Number: BQ40Z50-R2 Other Parts Discussed in Thread: BQ27510EVM , BQ40Z50 Hi I have the BQ40Z50EVM wired to a 4S pack with an ELOAD for discharge and the BQ27510EVM for charge. I have attempted multiple times to perform the learning cycle and seem…
Part Number: BQ40Z50-R2 Other Parts Discussed in Thread: GPCCHEM Issue 1: Currently, we are encountering a problem of insufficient SOH (State of Health) and the updated Qmax reading is too low. However, the actual capacity of the battery itself is sufficient…
Part Number: BQ40Z50-R2 Hello,
My customer wants to receive the BQ40Z50-R2 device with the BQ40Z50-R5 firmware pre-installed when he purchases it.
Is there any way to purchase a device with the BQ40Z50-R5 firmware pre-installed? Or do users have to…
Part Number: BQ40Z50-R2 Tool/software: The recommended battery connection order for bq40Z50-R2 is VSS-->VC1-->VC2-->VC3-->VC4/BAT or connect to VSS first and the others don't need to be in order.
Part Number: BQ40Z50-R2 Hello,
We are currently working on the bq40z50-r2 and using a 4S3P cell configuration. When the battery pack goes into deep discharge, it does not initiate charging again. There is no voltage present at the pack terminals (PACK…
Part Number: BQ40Z50-R2 Hello,
If I upload the .srec file from a 4S3P cell pack into a 4S1P cell pack, then I reset the Update Status from 0E. It goes back to 00, but after doing 'Write All' it again changes to 0x04. Is this the correct method for resetting…