Part Number: BQ40Z50-R2 Tool/software: Hi,
this question is related to: https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1508019/bq40z50-r2-rsoc-locked-at-99-100
Since i can not unlock the thread i opend…
Part Number: BQ40Z50-R2 hi Team,
customer has questions on the SOH temp a/k DF parameter settings.
from the TRM it describes that the SOH FCC calculation will be using SOH temp a and SOH temp k.
why do we need a separate SOH temp a and SOH temp…
Part Number: BQ40Z50-R2 hi Team,
for design considerations
customer would like to check what's the maximum pull high voltage for the PRES pin
in the Datasheet, there is only MIN value
for device bq40z50-R2
Thanks
Part Number: BQ40Z50-R2 What is the acccuracy of total firmware runtime in Lifetime of the fuel gauge IC. Example, if the battery pack is assembled in 10 March 2028 and lifetime is enabled, will the number of hours after 5 days will be the same as recorded…
Part Number: BQ40Z50-R2 Dear Sir/Madam,
We are a company, Asankhya AI Private Limited, currently working on the development of a 5-parameter patient monitoring system.
We would like your support in selecting a suitable power path controller for our…
Part Number: BQ40Z50-R2 Tool/software: I want to develop a battery pack with a capacity of 100Ah using 5Ah cells in a 3S20P configuration.
If I use bq40z50-r2, the maximum capacity is not suitable for 65Ah.
Can I adjust the scale factor to use it…
Part Number: BQ40Z50-R2 Other Parts Discussed in Thread: BQ40Z50 , BQ34Z100-G1 Hi,
As BQ40Z50 has 16-bit register for current sensing, scaling method was proposed.
bq34z100-G1 High Cell Count and High Capacity Applications
"The data flash configuration…
Part Number: BQ40Z50-R2 Other Parts Discussed in Thread: BQ40Z50 Hi TI Team,
I am using the BQ40Z50, which currently supports up to 4 TS pins for NTC temperature measurement.
Is there any recommended external expander IC or circuit that can increase…
Part Number: BQ40Z50-R2 Hi!
Regarding the POR described in the procedures for BQkey programmer, is sending a command for device reset enough or we need to put the battery to shutdown mode? if it is necessary to put it to shutdown mode, is a shutdown…
Part Number: BQ40Z50-R2 Other Parts Discussed in Thread: BQSTUDIO Hello all,
A would like to know if it's possible to configure somes views/onglets in BqStudio ?
I explain: I would like to reduce the number of commands present on commands onglet or…