Part Number: BQ41Z50 Other Parts Discussed in Thread: BQSTUDIO A question for Current Wake Detector SPEC as the following info.
SPEC show the setting 0x70 = 0.5mV in charge, but 0x71 = -0.5mV in discharge.
So I’d like to double check the it’s SPEC…
Part Number: BQ41Z50 Other Parts Discussed in Thread: BQSTUDIO
Hi:
I am a bit confused by the datasheet.
my quesiton is what is the internal CC current sampling chain and how to set default value of CC_Gain.
My cal is here:
based on datasheet…
Part Number: BQ41Z50 Dear Sirs and Madams,
We understand that when the BQ41Z50's GPIO is configured as an input, it is set to pull-up; is it not possible to configure it for pull-down instead?
Regards,
Masashi
Part Number: BQ41Z50 Other Parts Discussed in Thread: BQSTUDIO , , EV2400 I am trying to communicate with a bq41z50 with an ev2400 using the test version (1.3.130) of bqstudio but I unable to communicate. I am selecting the 4150_0_01 bqz file and seeing…
Part Number: BQ41Z50 Hi TI team,
I have a question for you:
What issues would occur if the SMBD and SMBC pins on the BMS (BQ41Z50) are short-circuited while it is not connected to the system?
Best Regards,
Peter
Part Number: BQ41Z50 Other Parts Discussed in Thread: BQSTUDIO The data can only show the capacity up to 2348mAh (50% of the pack capacity) and the max discharging current 32A (50% of max 64A). However, it should be the actual capacity and discharge current…
Part Number: BQ41Z50 Other Parts Discussed in Thread: BQSTUDIO Hi,
We are working with the BQ41Z50 inside our battery pack. We have performed some configuration, learning cycles and ChemID selection in BQStudio. We are satisfied with the configuration…
Part Number: BQ41Z50 Other Parts Discussed in Thread: BQSTUDIO Hi, everyone ;
After replacing the BQ41Z50 on the BQ41Z50 EVM ,the Cell 4 Voltage on the Register page in BQStudio has no readings .(I'm currently using the BQ41Z50 EVM,the FW is 4150_0_01…
Part Number: BQ41Z50 Other Parts Discussed in Thread: EV2400 When operating batteries at very cold temperatures we noted that communication is lost to the chipset, even though the battery output remains enabled and working normally.
We have taken many…
Part Number: BQ41Z50 Hi,
I am trying to evaluate the TI BQ41Z50 using the BQ2400 along with the BQ41Z50EVM. I managed to download and run the BQ41Z50 configuration for battery management studio. Reading registers and setting some values work fine. …