Hi Al
" So I have this switch that when it gets activated the charging would start."
" I assume the the BQ50002A and the BQ500511A would automatically stop the wireless charging when the battery pack hits the 100% mark. " -- Bill J - The TX…
Hi Daniel
I have captured a typical start up waveform, below.
CH1 / Yellow is RECT voltage.
CH2 / Red is CHG pin voltage
CH3 / Blue is BATT voltage
CH4 / Green is BATT current
Test were done with standard EVM and BQ50002A / 511A TX EVM.
In your waveform…
The snubbed would add a load to the bq50002A and increase thermal rise. Hard to say if this is the only cause of device heating up that you are seeing.
Part Number: BQ500511A Other Parts Discussed in Thread: BQ50002A , BQ500511 , BQ50002 , BQ25100 , BQ51003 Hi,
I am struggling to find the difference between the bq500511/bq50002 and the bq500511A/bq50002A combination.
The only thing I seem to find in the…
Part Number: BQ51051B Other Parts Discussed in Thread: BQ500212A , BQ500511A , BQ50002A Hi Sir
if BQ51051B charge done
May I know TX board will indicate charge done or not ? or have any method can let TX board to know RX is going to charge done ?
Tha…
Hi,
I need to know if the BQ500511A and BQ50002A is available in your production for the 10 years on the futur?
Thank you for you answer.
Best regards.
Lionel
Part Number: BQ500511A Other Parts Discussed in Thread: BQ51003 , BQ50002A Hi,
We are using the BQ500511A in combination with the BQ50002A for a wireless charger in combination with the BQ51003 on the receiver side. We noticed a strange error state which…