Other Parts Discussed in Thread: BQ51013 , BQ500210 Hi,
I am trying to use off the shelf A10 coil (24uH) as the receiver for a WPT solution. I am using bq51013 at the receiver side and bq500210 at the transmitter side.I use A10 coil at the transmitter…
Hi Dick,
I have to wait for answer from coils vendor. But besides coils I need controllers and I would like to test them as soon as possible with EVM :) Is it good idea to choose them, when I don't have coils?
For receiver part I think BQ51013A…
Other Parts Discussed in Thread: BQ500210 , BQ51013 Are there any test reports or data available for EMC emissions for the bq500210 and BQ51013 EVM's available, CE or FCC?
Thanks
Hello Gianluca
The bq500210EVM-689 is our 19V input TX, WPC TX type A1 or A10. The coil should have an inductance in the range of 24uH. Also low DCR is desirable.
TX is a resonant converter topology and even with no load on the RX the circulating…
Other Parts Discussed in Thread: BQ500210 , BQ500212A
3146.bqTESLA TX Sleep Mode -- MSP430 Based.pdf
The bqTESLA Transmitter (TX) will use Sleep Mode to reduce input power when no Receiver (RX) is present. We have two methods for doing this one is…
Julian,
Did you lower the input voltage for BQ500210 EVM? The 760308201 coil has only 15 turns while the original TX coil has 20. The voltage on the receiver side can be too high tripping OVP if you tune TX resoancne to 100kHz. Alternatively to lowering…
Francesca,
When the bq500210 receives the charge complete signal, it will not attempt to restart for 5 minutes (see section ADVANCED CHARGE INDICATION SCHEMES in the datasheet). Have you verified the 5 minutes has expired? Each time the timer expires…
Other Parts Discussed in Thread: BQ500210 , BQ51013A , BQ51014 Hi,
I am using bq500210 and bq51013A for a battery charging solution.
I have a 42.2kOhm between ground and pin 44 (LED_MODE). According to the table in the datasheet of bq500210 this corresponds…
Dear Bill,
Thank you very much for your help and answer.
I am interested about this component due to its reduced cost components, which will help us from the very beginning to aim for a low cost design and because it has couple of new features compared…