Hi Kaan
Support for the BQ500212A is very limited, the device is NRND.
If you contact me using the conversation feature of the forum I will do what I can.
Part Number: BQ500212A Other Parts Discussed in Thread: BQ51050B Hi team,
Customer is searching a wireless charging solution that can support Qi and constant communication during charging. I was wondering if BQ51050B and BQ500212A can work. Besides, is…
Part Number: BQ500212A Hi Expert,
Since BQ500212A is NRND, do we have new similar wireless transmitter device? Also do we have automotive device? It would be great that you can send me the roadmap. Thanks!
BR,
Elec Cheng
Part Number: BQ500212A Other Parts Discussed in Thread: BQ51013B-Q1 Hi, I need to know if your wireless charging IC has low latency communication through induced charging. In addition to loading, is it possible to send a personalized message by me between…
Part Number: BQ500212A Other Parts Discussed in Thread: BQ51050B I have to design a new product which should be based on the BQ500212A but it's end of life. I am using the BQ51050B receiver and would like to know which transmitter should be used.
…
Part Number: BQ500212A According to the I2C interface note, there is a control error byte in block 0xD0. As noted, it is updated frequently. When a device is charging steadily it seems to be switching between 8 and 9. The device I'm working on is having…
Part Number: BQ500212A Hi, Good day. Our customer is debugging their design that uses the BQ500212A. With this, they are looking for the "bqTesla TX Tuning Tool". Can you please help us provide this to them? Thank you . Regards, Cedrick
Good to hear you are running charge cycles.
Do not have any EMI application notes. But a very common approach is to layout the PCB to the dimensions of coil so that it will fold under coil then it acts as a shield.
Part Number: BQ500212A Hi,
I am working with BQ500212A-EVM board for testing wireless power transfer. I am using B51013B-EVM as receiver. I want to confirm that I can source 1A from the RX module before I continue. I use a variable current load circuit…