Part Number: BQ500212A Hello,
this is just a small "heads up": In figure 2 of the user guide "bq500212A bqTESLA Wireless Power TX EVM (Rev. C)", T_Sense is connected between a fixed value resistor and a NTC. If this NTC is missing or has a cold joint…
Part Number: USB-TO-GPIO2 Other Parts Discussed in Thread: BQ500212A Hello,
We just purchased the TI USB-TO-GPIO2 and we’re using it to connect to the I2C bus of a wireless charger using the TI chipset bq500212a (as identified in the screenshot below…
Part Number: BQ500212A Dear team,
My customer is looking for Qi certified wireless power transmitter and I have promoted BQ500212A but would like to have more electric-generating capacity.
Do we have any proposal for this request?
Regards,
Hello
A transmitter designed with the BQ500212A will probably meet WPC 1.2 standard. Many requirements are external of the IC. The changes from WPC 1.1 to 1.2 for 5W systems, now called Baseline Power Profile are minor and the BQ500212A will meet them…
Part Number: BQ500212A Dear Supporting team,
For my bq500212a, the gate and coil voltage signal is fine as the datasheet with 80ms pulse and 300ms rest under led mode 2.
The led2 keep ON and led1 and 3 are Off which response as fault.
Two behavior are…
Part Number: BQ500212A Other Parts Discussed in Thread: BQ51003
Hello,
I was testing the Bq500212A and BQ51003 EVM modules and was checking for the efficiency.
Following the Bq500212A EVM test procedure, I supplied 5V and 3A current limit at J1 and…
Part Number: BQ500212A Other Parts Discussed in Thread: BQ2000 , BQ51013B Hi,
Now we use BQ500212A(TX) to BQ51013B(RX)+BQ2000 for NiMh Battery Charger application and BQ2000 charger timer setup to 7hr.
Then we find our PCB Board that it is auto stop to…
Part Number: BQ500212A Other Parts Discussed in Thread: BQ51003 , BQ50002A Hello,
I've used the evaluation board: BQ500212AEVM-550. I've removed the coil and replaced the coil oith TDK coil wt151512-22f2-id
https://product.tdk.com/info/en/catalog…
Part Number: BQ500212A We are creating a Qi charger for our product we are designing. I bought the bq500212a dev board but digikey says that IC shoudl not be used in new disigns. What should be used instead?