Part Number: BQ500511 Other Parts Discussed in Thread: EV2400 , BQ50002A , , BQSTUDIO Hello! Use the transmitter chips bq500511 and bq50002a, the receiver is implemented on a chip BQ51050. I work with the chip bq500511 using EV2400.
1. How is the calculation…
Other Parts Discussed in Thread: BQ500511A , BQ50002 , BQ50002A , BQ500511 Part Numbers: BQ500511, BQ500511A, BQ50002 and BQ50002A
Hi,
BQ500511, BQ500511A, BQ50002 and BQ50002A are NRND, however in older threads I've seen that TI is not planning to make these…
Other Parts Discussed in Thread: BQ500511 , BQ50002 , BQ50002A , BQ500511A , TIDA-00623 HI,
Actually, we have a Product that use your circuit Bq500511 and BQ50002. we have decided to remake our product and we have seen this instruction “NRND” on web site.…
Part Number: BQ500511 Other Parts Discussed in Thread: BQ50002A Hi
We are using BQ50002A BQ500511A to construct a wireless charging solution for mobile phone.
The charging is available, but the input current is only about 0.2A.
We use a DC power source…
Part Number: BQ50002 Other Parts Discussed in Thread: BQ500511 , , BQ51013 , BQ51013B , , BQ500511A Hi,
I've noticed that the BQ50002 wireless power transmitter and BQ500511 controller are not recommended for new designs. Are there replacements for these…
Part Number: BQ500511 Other Parts Discussed in Thread: BQ50002A , BQ50002 Hi
I have a 5W design based on the bq50002 + bq500511 with the design itself based almost identically on the reference design of TI - other than a few board size changes.
With the latest…
Part Number: BQ500511 Other Parts Discussed in Thread: BQ50002 The problem occurs when I use bq50002EVM-607 or BQ500511+BQ50002:
After the battery is fully charged, the green LED on the power transmitter lights up:
And then, I repeat the following steps…
If no RX present the unit will be in a standby mode and TX will ping the coil every 500mS to check for RX. Ping freq is 175kHz for about 80mS.
When the RX is in place and power transfer has started the freq will vary with load. Light load will have…
Part Number: BQ500511 Other Parts Discussed in Thread: BQ50002A , Hi
1.
According to the datasheet, it is offered that LED_A/B/C pins are connected to LED via 1Kohm resistor.
Is it possible to use a resistor smaller than 1Kohm?
2.
What is the maximum…